How can i enable SYSCFG in STM32WB55RG board
Hello,Could you tell me how can i enable clock access to SYSCFG in STM32WB55RG board, because i couldn't find the proper bit to enable SYSCFG in APBENR registers in the reference manual
Hello,Could you tell me how can i enable clock access to SYSCFG in STM32WB55RG board, because i couldn't find the proper bit to enable SYSCFG in APBENR registers in the reference manual
Hello...I am using a Nucleo WB55 board. I can run the FLASH_EraseProgram that comes with the WB55 example code successfully. I have pre-existing code and am trying to pull this into my code. I have checked the PWR and the Flash SFR in the debugger...
Hello everyone, I am working with 3 stm32wl55JC module. 1 is receiver the other 2 is transmitter. The code has UTIL_SEQ_RegTask((1 << CFG_SEQ_Task_Sensor_Process), 0, Sensor_Process);I want to add another task which needs to work as endless loop....
If I comment out "MX_LoRaWAN_Process();" in main, then the USART1 interrupts trigger as they normally would. Could anyone offer some advice of how to add USART1 to the example?Kind regards
Hi,I'm using STM32WB5MMG and want to send 8-bit data through BLE every specified duration (e.g. 1s). I have tested the Bluetooth and timer interrupt separately and both works fine. However, when I tried to trigger the Bluetooth using timer interrupt ...
My expectation was that a pin-interrupt using EXTI will lead to wakeup times just slightly longer than the wakeup delays named in the datasheet (below 10µs), but what I see is this (falling edge on yellow finally reached the ISR on the magenta rising...
Hi,I want to enable the SYSCGF in STM32WB55RGV6 , but when ı look the reference manuel; it says that SYSCFG is on the APB2 bus however when look the APB2ENR register there is nothing about SYSCFG . What should ı do to enable SYSCFG?
Hi Team,Need the RTC Code base with LSE or LSI as clock source and needs to get the interrupt at every 1sec rate. Is there any example code with these settings. Please share the code base or any example project, those are very much useful to us.Regar...