STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 220 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4065 Views
  • 0 replies
  • 3 kudos

Resolved! How to identify two or more BLE devices

Hi, I have a question.I am developing a BLE HIID device using the STM32WB55 evaluation board.I am not sure how to identify multiple devices with the same firmware loaded.The problem I am currently encountering is as follows ↓↓↓.Prepare two CFG_STATIC...

ELEHM by Associate II
  • 2261 Views
  • 3 replies
  • 1 kudos

Resolved! STM32WB55 - input clock for TIM6?

 I am using STM32WB55 with 32 MHz HSE and am trying to find out which input clock frequency I should use for TIM16. Unfortunately it is not clear in the diagram from the datasheet. Where can I get this information? Greetings,Andreas   

AndreasC_0-1721736526957.png
AndreasC by Associate II
  • 2481 Views
  • 4 replies
  • 2 kudos

BLE Router and Server

I have two STM32WB5MM- DK . Using an example for a diffrent board I have configured one of them as router and other as server. I dont know if they are getting connected.  I need to connect these exclusively and then connect the router to Mobile phone...

Rituraj by Senior
  • 1982 Views
  • 6 replies
  • 0 kudos

Resolved! STM32WBA55G-DK1 not compatible with all mobiles

Hi I recently purchased DK board and connected to the phone to check the dumped code.But, I couldn't listen to any music nor call. I realised only few selected mobiles with BLE Audio can be used to test the board.Any solution to this? @STTwo-32 @KDJE...

Pallavi by Associate III
  • 2235 Views
  • 3 replies
  • 0 kudos

Resolved! BLE of STM32WBA55

Iam using STM32WBA55 and i tried to configure STM32_WPAN BLE application but the generated code has a file not found error.ask me for any further details regarding this problem because i don't know what to put in my post that might help in this probl...

image.png

Resolved! Writing my own ID into flash

Hello,I want to write my own ID in the STM32WL55 memory. For this I use STM32Cubeprogram and the ST-LINK V3.My question is: is there a small flash area where I can write this identifier and which does not interfere with the code and data so as not to...

laesser by Associate II
  • 2388 Views
  • 4 replies
  • 2 kudos

STM32WB15 Dissapointment

Hi,I just have to voice my opinion on STM32's BLE STM32WB15 solution I have got, out of the box (Nucleo-WB15CC) I have spent many hours now just trying to get a simple example started just advertising to a mobile but I still can't get it too detect. ...

PLee.3 by Associate III
  • 2577 Views
  • 5 replies
  • 3 kudos

Resolved! STM32 Bluetooth Classic MCU

Hi, I am wondering if you can get STM32 MCU with integrated Bluetooth Classic as the only examples I have found (Like WB55) are all bluetooth low energy? 

Linkpad by Associate III
  • 3454 Views
  • 5 replies
  • 3 kudos