cancel
Showing results for 
Search instead for 
Did you mean: 

STM32WL FM Modulation

Jò
Associate

Hello,

I just came accross the STM32WL series and I was wondering if I can implement a different modulation other than the ones included (FSK, PSK).

I need to acquire an analog signal, convert it to digital and then modulate it with a frequency modulation and up-convert it and send it trough the PA. Can I do that using one of the STM32WL?

Thanks.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello @Jò and welcome to the ST Community :smiling_face_with_smiling_eyes:.

Our STM32WL series support LoRa, (G)FSK, (G)MSK and BPSK modulations. For more details, you can refer to the STM32WL documentations available on this link.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
STTwo-32
ST Employee

Hello @Jò and welcome to the ST Community :smiling_face_with_smiling_eyes:.

Our STM32WL series support LoRa, (G)FSK, (G)MSK and BPSK modulations. For more details, you can refer to the STM32WL documentations available on this link.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.