MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

lis2de12 landscape/portrait interrupt

I have this MEMS sensor on a custom board to detect landscape or portrait mode of my device.The problem is that it doesn't generate an interrupt.- 4D mode should be sufficient.- Range 2g- Tested different ODR settings. My current code is now:     voi...

Capture545454594.PNG
WSpar.1 by Associate III
  • 994 Views
  • 2 replies
  • 0 kudos

Resolved! Mems AR

Anybody know where I can get the data sheet for MEMS AR products and how can I purchase it?Thank you.

Clint100 by Associate
  • 2570 Views
  • 3 replies
  • 1 kudos

LSM6DSV16X getting started

I have the Sparkfun version of the LSM6DSV16X. I used it with the Arduino IDE and everything works easily. I migrated that LSM6DSV16X board to using a Nordic nrf5340dk. There doesn't seem to be a working library for the LSM6DSV16X, but that is ok as ...

mej by Associate II
  • 2735 Views
  • 4 replies
  • 0 kudos

Configure a IIS328DQ to replace a LIS3LV02DQ

I have used the LIS3LV02DQ before but it is no longer being made. A new circuit has the IIS328DQ but I can not get it to work as the did. I can successfully get the WHO_AM_I to return and set/read the control registers so I know the SPI is working fi...

GPres.1 by Associate
  • 630 Views
  • 1 replies
  • 0 kudos

ASM330LHH

While I’m using ASM330LHH the gyroscope’s data jump to unusual value just once sometimes . The data rate is 10hz 

IMG_1599.jpeg
Mal by Associate
  • 690 Views
  • 1 replies
  • 0 kudos

LSM6DS032 programming finite state machine

Hi all, I'm trying to move Finite State Machine config from devkit using Unico GUI to final application. I've prepared movement wakeup example from FSM datasheet in Unico, which is working totally fine on devkit, it could even detect knocking in desk...

Zrzut ekranu 2024-02-05 113640.png
mpopko by Associate II
  • 2426 Views
  • 5 replies
  • 0 kudos

IIS2DH INT1 signal generation

Posted on June 12, 2017 at 11:07Hi,I have inserted the accelerometer in a custom board.Is is connected via I2C to a microcontroller, Vdd and Vdd_IO both connected to 3V3.In my application the micro controller awakes when the acceleration on all the ...