MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STHS34PF80 Sensor's Power Consumption is very high.

Hello there, I am currently working on a project where I am prototyping STM32WL55 with an STHS34PF80 sensor to detect the presence. The presence detection is excellent and robust so far. However, the power consumption seems to be very high at the mom...

Can‘t pair with BLE Sensor Tile.Box Pro

I am not able to pair Sensor Tile.Box Pro with my iphone 13 over Bluetooth with the app ST BLE Sensor. When connecting I get prompted to enter number shown on the device, but the Tile.Box does not have a display, so that’s impossible. 

michal6 by Associate
  • 934 Views
  • 0 replies
  • 0 kudos

6-positions calibration

Hello,     I am developing on a custom boards with a STM32F407, LSM6dsv16x and LIS2MDL.On CubeMX I set the MotionFX package. Even selecting the MotionAC it looks like the library is not added to the output (is it correct?). The motionTL can be added....

MRaff.1 by Associate III
  • 1162 Views
  • 0 replies
  • 0 kudos

Run time fault detection in ASM330LHB

Hi,    I am using ASM330LHB in my project. ASM330LHB has only built self test which can only executed during power on to see ASM330LHB is healthy or faulty? But during runtime (device working in dynamic conditions) there is no way to find ASM330LHB i...

Pavani by Associate II
  • 1526 Views
  • 2 replies
  • 0 kudos

STHS34PF80 Abnormal operation

When STHS34PF80 detects the human body for a period of time, TPRESENCE cannot fall back normally, and pres_flag is always 1。 code:

top_0-1711014368016.png
top by Associate
  • 1908 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.