MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Including motion fx library in a third party arm mcu

Hello,for a new project we are avalutaing the use of an iNEMO inertial module in conjunction with the motion fx library with the goal of doing position estimation with dead reckoning.My doubt is about the library, since we are forced to use a thrid p...

DGiov.1 by Associate III
  • 2094 Views
  • 4 replies
  • 0 kudos

Resolved! LIS3MDL AMR

Hello,I searched the forum and found out a topic regarding the sensing technology of LIS3MDL sensor. The topic mentioned that LIS3MDL is a TMR sensor, however no support documents are included to further investigate the integrated circuit of the sens...

NiSpan by Associate
  • 1310 Views
  • 1 replies
  • 0 kudos

Resolved! ECompass debagging impossible.

Hello,can anyone tell me what I am doing wrong?For example, I can't get app_mems.c (eCompass) to debug.The debugger does not stop when I set a breakpoint on subsequent function calls because, for whatever reason, the “SensorReadRequest” always has th...

RGünt.1 by Associate II
  • 1390 Views
  • 3 replies
  • 0 kudos

LSM6DSM instability and high current consumption

We have an issue with LSM6DSM and LSM6DSV. Sometimes they start consuming abnormally high current of 2.5 mA, which is about 200 times more than normal. Most reliably this can be reproduced when their SPI clock input pin 13 is driven by a week 47k pul...

IIvan.22 by Associate III
  • 1201 Views
  • 0 replies
  • 0 kudos

LIS3DSH - analogue to digital converter

Posted on October 16, 2016 at 11:59The LIS3DSH has a three channel 10 bit A/D converter but I can't find any information on it. What is the accuracy? (I could tie one channel to a voltage reference for calibration if necessary) What is the input vo...

LSM6DSO

Hi, community,   I have a bespoke board running an rp2040 and have been coding the LSM6DSO from the spec, along with using web-found python and cpp examples as starter code. There are several things I haven't found enough detail on and would like hel...

LSM6DSV - temperature issue

Hello,I am trying to get the temperature from LSM6DSVX sensor. Accel and gyro are working well but I can't get the temperature. The buffer cannot be enable for temperature. It works for Accel  and gyro buffer can be enable.their is something specific...

AlexBT by Associate
  • 1588 Views
  • 3 replies
  • 0 kudos

How to improve step count or pedometer accuracy?

Hello Team ST and Community,I have following code for step count for our wrist-based device. We use LSM6DSO IMU.The step debounce threshold has improved the step count accuracy. It is currently set to 20. But, I could not get rid of the false positiv...

ASoni.2 by Associate III
  • 1403 Views
  • 1 replies
  • 0 kudos