I am trying to use the DATALOG1_V1.1.0\Utilities\Python_SDKWhen I call the script hsdatalog_data_export I get an error: "No module named 'click'What to do to make these scrpits work? Pyhton is V3.7.8
I tried out the STBB1 with the evalboard to drive a load of 500mA.My trials were successfull. I did them by switching on my power supply with 5V and afterwards I was switching the 500mA Load on and off at the output. -> everything cool.Now I have my ...
During serveral trials, when switching between STLink and UART setup the programm cannot be ended anymore. I can operate it, but I have to kill it with the taskmanager to quit.AltF4 and so on is not working,.Win7 x64
I had Pyton V2.7 installed from another project, and this was blocking the V3.7 Python to install correctly.After uninstalling all and reinstall V3.7.9, I was able to run the pip installation of the needed modules.So now the scripts are working fine....