User Activity

Hello,I'm working on an ultra low power application where the MLC of the LSM6DSO32X is used to wake up the mcu when interesting stuff is happening, in particular I implemented two decision trees, each one focused on the detection of a pattern.In orde...
Hello,I'm looking for the drivers for the LSM6DSO32X. In the example code I found the drivers for LSM6DSO32 and for LSM6DSOX which are similar but not identical. Are them available somewhere?Davide
Hello,I'm working on a ultra low power application using the LSM6DSO32X. The goal is to have a device that reacts (with a short radio message) when its orientation relative to gravity changes. For this I wish to use as much as possible the FSM and th...
Hello,I'm integrating the LSM6DSO32 into an MCU project and I'm using the example drivers from CubeMx.The problem is that I don't understand how the gyroscope sensitivity is calulated into the drivers. The constants for the sensitivities at the vario...
Hello,for a new project we are avalutaing the use of an iNEMO inertial module in conjunction with the motion fx library with the goal of doing position estimation with dead reckoning.My doubt is about the library, since we are forced to use a thrid p...