MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LSM6DS3 Gyroscope Shock Immunity

Greetings. I have been working on a product research project for about a year and a half. The project involved some mechanical problem solving to get to the point of testing that I am at now.The LSM6DS3 is embedded in a solid object at rest in an unk...

Nate by Associate
  • 706 Views
  • 0 replies
  • 0 kudos

How to transmit and receive data between Arduino HC-06/HC-05 and bluenrg-ms on the BLE bluetooth in the STEVAL-STLCS01V1 SensorTile

Hello.In my project i need to send commands from my control station (Arduino Mega) with the HC-06 (or HC-05) bluetooth module, to the STEVAL-STLCS01V1 SensorTile BLE bluetooth sensor.An example of a command i want to send:Command: GET_TEMPData sent b...

RFink by Associate II
  • 732 Views
  • 0 replies
  • 1 kudos

Resolved! How to detect drop of a product

What would be a good accelerometer to be used in a product to detect if it has been dropped? The idea is to build a battery-powered subsystem for an (expensive) medical equipment to track improper handling (e.g. drop or tilt) during transport or duri...

LPS331AP averaging algorithm

Hello.Concerning LPS331AP's RES_CONF register and its AVGT/AVGP bits: what is the frequency the corresponding internal averaging is being performed? Does it depend on selected output data rate? How is the averaging applied when the device is in one-s...

vech2001 by Associate II
  • 1157 Views
  • 4 replies
  • 0 kudos

steval-idp005v1 interface with Nucleo board

I am working with STEVAL-IDP005V1 and Nucleo64 boards and STEVAL board already programmed, i interface STEVAL-IDP005V1 to ST-LINK of nucleo board & i drop-drag the .bin file into disk but not able to get the output on serial monitorThe STEVAL-IDP005...

v_1 by Associate II
  • 473 Views
  • 0 replies
  • 0 kudos

Sampling frequency of ACC GYRO and MAG for MotionFX

Hello in my project I use LSM6DS3TR and LIS3MDLTR.The data from MEMS is processed by MotionFX.How high should the sampling rate of LIS3MDLTR be?How best should I synchronize the data before coming to the MotionFX?The program runs on the stm32l452 mic...

YL by Associate II
  • 1234 Views
  • 4 replies
  • 0 kudos