cancel
Showing results for 
Search instead for 
Did you mean: 

How to transmit and receive data between Arduino HC-06/HC-05 and bluenrg-ms on the BLE bluetooth in the STEVAL-STLCS01V1 SensorTile

RFink
Associate II

Hello.

In my project i need to send commands from my control station (Arduino Mega) with the HC-06 (or HC-05) bluetooth module, to the STEVAL-STLCS01V1 SensorTile BLE bluetooth sensor.

An example of a command i want to send:

Command: GET_TEMP

Data sent back from the SensorTile to the HC-06 on the control station: the temperature measurement

When i looked on google, i saw that the only way to get the sensors measurements is via a an app. but i want to create new commands and receive the sensors measurements to my control station (the Arduino Mega with the HC-06 or HC-05 bluetooth module).

How can i create new commands and send and receive data between the HC-06/05 and the STEVAL-STLCS01V1 SensorTile BLE bluetooth sensor?

Thank you for your help,

Reshef Finkelstein

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0