MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LSM6dsl interrupt on axis threshold

There is any workaround for doing this with a LSM6DSL? I understand the available interruptions like WAKE_UP, significant movement,4D, 6D..... are designed for other kind of uses, mainly smartphones and wearables.But I need an interruption old-style...

David LR by Associate II
  • 682 Views
  • 1 replies
  • 0 kudos

Resolved! LIS2DE12 interrupt configuration

I am currently working on the LIS2DE12 accelerometer. I've been reading the datasheet and I was a little confused with the interrupt configuration. The datasheet says the device provides 2 interupt pins (INT1 and INT2). 1. My understanding is that yo...

There seems to be some conflicting information in the VL53L1X API documentation regarding min timing values for 'Timing Budget' and 'Inter Measurement Period'.

 The general API user guide, UM2356 (rev 2), says that the min timing budget is 20ms, but the ultra-lite driver guide, UM2510 (rev2), says 15ms is the minimum. I've tested with 15ms (I'm using the ULD) and it seems to work fine, but just wanted to ma...

RSarv by Associate
  • 527 Views
  • 1 replies
  • 0 kudos

VL6180X Not working with 10KHz I2C Frequency

Dear members,I am currently trying to interface Arduino Atmega 328p with VL6180X via I2C Bus. I have prepared basic code for reading Range value in single shot and continuous  mode, it is working file. Now I changed I2C SCL to 100 KHz, 50 KHz, 20 KH...

VKulk.8 by Associate
  • 605 Views
  • 1 replies
  • 0 kudos

VL53L1X overshoot?

In my initial testing with the VL53L1X, I'm seeing that by rotating the sensor from directly facing an object to facing the ceiling, which is well over the max distance away (I'm operating in 'short' mode, so that should be 1.3m), I get spikes up to ...

RSarv by Associate
  • 2426 Views
  • 1 replies
  • 0 kudos

LPS33HW only responding once on SPI

Hello,I'm having some trouble with an LPS33HW. It only responds to a single WHOAMI message after powerup or MCU reset (ie via the NRESET line)

0690X000008j1lJQAQ.png
DAllo by Associate II
  • 640 Views
  • 1 replies
  • 0 kudos

Resolved! Accelerometer for machine monitoring

I am looking for an accelerometer we can use for motor condition monitoring. Which one would you recommend ?NOTE: This question and answer originated from a customer support case which was handled by us. We regularly review support cases and add any ...