MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS2DH 6D mode not working properly

Hello,I am trying to implement 6D mode. I am following 1:1 the code documented in the design tip DT0097.I have been trying for a while: I2C interface is working and other modes of LIS2DH work properly.As a safety measure, during the init I reset all ...

vcaia.1 by Associate II
  • 1708 Views
  • 6 replies
  • 0 kudos

MEMS Accelerometer application

HI Guys, I am looking for the MEMS Accelero meter for measuring the vibration in textile machines. Whether ST has the application example for condition monitoring system in machine or industrial automation.If so please share the details

NGopa.1 by Associate II
  • 2155 Views
  • 5 replies
  • 0 kudos

Resolved! MotionAR Initialize function gets stuck

Posted on January 24, 2018 at 17:10I am trying to add MotionAR library to a DataLogger sample application running on SensorTile. I manager to compile the library and program my chip with it. Near the top of my main() I added simple MotionAR_Initiali...

0690X00000609PBQAY.png
Norman S by Associate II
  • 2227 Views
  • 3 replies
  • 1 kudos

I'm want to acquire rawdata from the SensorTile.box (Steval$MKSBOX1V1). Using the app, I can get 16bits output raw data when Bluetooth streaming and then sending the files to email, but it's very limited.

How to I get control over the output data format? Is there a way I can upgrade the firmware, without any additional hardware (just using USB cable and STM32Cube IDE or Programmer) to change how I record the data?

MMarq.1 by Associate
  • 1839 Views
  • 3 replies
  • 0 kudos

how to configure threhold based interrupt in LPS25HB

hello,i m trying to  generate an interrupt event based on a defined threshold to wakeup the mcu from stop modehere is my function to enable this feature void LPS25_interrupt_Config(){   Conf_reg1 |= (LPS25HB_CTRL_REG1_PD | LPS25HB_CTRL_REG1_ODR...

ATAYE.1 by Associate II
  • 3295 Views
  • 7 replies
  • 0 kudos

problem with acceleration amplitude in IIS2DH

HelloWe tested the IIS2DH sensor on a shaker.Accelerometer Settings:ODR = 5376Full-scale = +/- 16gLow-power mode.High-pass filter bypassedShaker Settings:frequency 1 kHzacceleration amplitude 13.592 gAs a result, the accelerometer registered an accel...

ESmir.1 by Associate
  • 1337 Views
  • 2 replies
  • 0 kudos