MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LSM303AGR give interrupt if movement falls below threshold.

For my project I want the LSM303AGR give me an interrupt if the read value of the X-axis falls BELOW the given threshold.For example:I have my threshold on 0.8.I bind the interrupt to to XLow and use movementrecognition.Now an interrupt is given if t...

Jvan .21 by Associate
  • 1236 Views
  • 1 replies
  • 0 kudos

Using LIS344ALH on STEVAL-MKI109V3 with Unico GUI 9.3.0.0

Hi guys.I am trying to used LIS344ALH on steval-mki109v3 with Unico GUI (v9.3.0.0).My first trial has been to connect my steval-mki109v3 with firmware V2.15.1 and Unico give me following Error message:Then I tried to connect to steval-mki109v3 after ...

0690X00000BvjeYQAR.jpg 0690X00000BvjfHQAR.jpg
Tino by Associate
  • 1085 Views
  • 1 replies
  • 0 kudos

LSM9DS1 I2C Write to r/w registers

I have an LSM9DS1 IMU/Magnetometer and I am having difficulty in writing a value to the control registers and reading it back after.I am using the I2C protocol with my MCU device set up as the master and the LSM9DS1 setup as the slave.1.      I am ab...

JFand.1 by Associate
  • 972 Views
  • 1 replies
  • 0 kudos

IIS3DWB - How to configure for wake-up interrupt?

First i pull both interrupt pins to GND before power up the sensor, as recommended by the datasheet. I then configure SDO pin with pull-up using register PIN_CTRL. Then i enable the accelerometer with no second filtering stage from register CTRL1_XL....

TResell by Associate II
  • 1584 Views
  • 1 replies
  • 0 kudos

LIS2DH12 position of 6D.

I use LIS2DH12 to determine the position of 6D. My task is to get interruption when the accelerometer is positioned with the + X axis at an angle of 50 degrees or more. Autumn X is also disabled. In this case, the acceleration along the X axis = 1g. ...

AGari by Associate II
  • 2412 Views
  • 7 replies
  • 0 kudos

Some general info on the SensorTile.box (TileBox) required

So, i can operate the sensor box, install the updates a couple different ways and generally get it to work. But, the TileBox has three switches on board, none of which are accessible from the outside without adding some holes to the case. The TileB...

TJM by Senior II
  • 2122 Views
  • 5 replies
  • 0 kudos