MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

MotionFX ALGO_FREQ

Hi,I am using the ism330dhcx and lis2mdl and run the MotionFX  algo.the ism330dhcx data rate is 104Hz and the lis2mdl is set to 100Hz (sensor hub ODR set to 104Hz)should i run MotionFX  algo at 100Hz or 104Hz ?on ST examples, when the ODR is set to 1...

malarab by Senior II
  • 459 Views
  • 3 replies
  • 0 kudos

Resolved! IMU with or withour magnetometer

HiI am not an IMU expert. My current task is to upgrade an old board which used LSM6DSL(gyro abd accelerometer ) and lsm303agr(Magnetometer) to caliculate orientation of a human head.As far as I can see LSM6DSV would be providing orientation data wit...

MK..1 by Associate III
  • 804 Views
  • 2 replies
  • 0 kudos

Resolved! ISM330DHCX Incorrect FIFO data / correct direct reading

[EDIT 03/04/25 09:15:35 AM] Well, it appears that, as usual, the real issue was sitting right in front of the keyboard… and could have been solved with a good old ‘Read The Freaking Manual.’ My deepest apologies for this classic case of user error! :...

Marconfr by Associate
  • 538 Views
  • 2 replies
  • 0 kudos

Is it possible to use Sensortile.box Pro with Pi Pico W?

Would it be possible to connect and send sensor data to a Pi Pico W from the STEVAL-MKBOXPRO? I’m looking for a way to connect them together via Bluetooth but a wired connection would be alright too. I have connected a Pico to the sensortile box via ...

spi1 by Associate
  • 414 Views
  • 2 replies
  • 0 kudos

Is my ASM330LHH imu sensor spi code correct?

I want to read acc and gyro data from my ASM330LHH sensor with spi communication, but I can't try the code because I don't have a sensor at the moment, can you take a look at the code, is there anything wrong or missing?(I selected the SPI_CS pin as ...

lis2dw12 linux driver difference

there are two kinds of linux driver for lis2dw12 in LIS2DW12 - 3轴MEMS加速度计,超低功耗,可配置单/双击识别,自由落体,唤醒,纵向/横向,6D/4D方向检测 - 意法半导体STMicroelectronics which is LinuxDriverIIO and LinuxDriverInput,1.what's the difference, which should we use, Do you have an appli...

xuehua by Associate
  • 482 Views
  • 1 replies
  • 0 kudos

Resolved! The differences between the IIS2DLPC and LIS2DW12

Could you tell me the differences between the IIS2DLPC and LIS2DW12?According to the reference URL, are there any differences between these two devices other than product longevity and guaranteed parameter values? I am particularly interested in whet...

MYabe.1 by Associate
  • 536 Views
  • 1 replies
  • 2 kudos

Resolved! SensorTile.box PRO : Record human activity and pedometer

Hello, @Andrea VITALI,After using the WESU board (https://community.st.com/t5/mems-sensors/lsm6ds3-lis3mdl-calibration/td-p/762534)we decided to move forward with the sensor tile box PRO. We want to record human activity recognition and pedometer inf...

pierre63 by Associate II
  • 3983 Views
  • 11 replies
  • 2 kudos