MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ILPS22QS pressure sensor holding SCL high

We have a ILPS22QS pressure sensor.We are getting an occasional i2c error.On investigation it seems the ILPS22QS sensor is holding the SCL line high during a pressure reading.I have read through the datasheet and see no functionality that would allow...

o0p3Ujx unnamed(1).jpg
mattc by Associate
  • 314 Views
  • 0 replies
  • 0 kudos

Cannot communicate with LSM6DSV with SPI nor I2C

I designed a small PCB for LSM6DSV but I got no signal on SPI-MISO and got NACK on I2C-SDA.I have replaced several chips but all the chips have the same behaviour(no signal reply).I'm very sure the SPI and I2C pins are correctly connected to LSM6DSV....

pansamic_0-1741676602183.png pansamic_1-1741676713794.png pansamic_2-1741676995350.png IMG_20250311_153603.jpg
pansamic by Associate
  • 534 Views
  • 0 replies
  • 0 kudos

LSM6DSOX MLC

Hi Team,  We are working with the LSM6DSOX sensor and integrating it with two different MCUs: nRF5340 and ATSAMD51, using the I2C communication protocol. We have been able to successfully read the device ID, accelerometer data, and gyroscope data. Ad...

LSM6DSOX MLC ActivityStates

Hi Team,  We are working with the LSM6DSOX sensor and integrating it with two different MCUs: nRF5340 and ATSAMD51, using the I2C communication protocol. We have been able to successfully read the device ID, accelerometer data, and gyroscope data. Ad...

Resolved! inertial module daisy chain via SPI

helloI need to interface about 20 small package inertial sensor via SPI and my MCU doesn't have enough GPIO for the chip selects so I'm looking for a module that can be daisy chained via SPI however I didn't find anything in the datasheets that indic...

Eddess by Associate II
  • 452 Views
  • 2 replies
  • 1 kudos

What does SensorHub actually DO?

We're using the LSM6DSV16X iNemo sensor and we're quite confused with the SensorHub feature (described in AN5763).Does this feature only store the external sensor data in the FIFO so that the main mcu doesn't have to read the other sensors directly? ...

MEMS audio sensor MP23DB01HP Values/Units

I have a question about the MEMS audio sensor MP23DB01HP. I think i already undertood that the output is a PDM, but my question is, how can I convert that to obtain a corresponding value in dB? Or some used unit? I have done the acquisitons, but know...

Resolved! LSM6DS3TR SEE framework drivers

Hello, We would like to integrate LSM6DS3TR sensor.For that to happed we need SEE (Secure Execution Environment) framework drivers for Qualcomm based processors. Could you please supply drivers for that? It is urgent. Thank you.Best regards,Miha

MApli.1 by Associate II
  • 433 Views
  • 2 replies
  • 0 kudos