MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS2DU12 Self-Test Not Producing Expected Deviation

Hello, I’m using the LIS2DU12 accelerometer and trying to perform the positive self-test exactly as described in the official application note. However, I’m consistently seeing results that do not meet the expected deviation thresholds, and the self-...

Resolved! MSL of accelerometer sensor

Hi,Where can I find inforamtion on Moisture sensitivity level for each sensors? I checked datasheets and few other documents in the product page but couldn't find it. I want to know the MSL of IIS3DWB.Best regards,Kev

KJose.1 by Associate III
  • 679 Views
  • 1 replies
  • 1 kudos

Resolved! STM32nucleo embedded STLINK for sensortile.box

Hi, i have a question, is it possible to use the embedded STLINK on the nucleo-f446re for programming the sensortile.box (steval-mksbox1v1) ? If so, how do i have to connects the pin? I have a JTAG Adapter v1.0 (included in the sensortile box), so i'...

alemezz by Associate
  • 724 Views
  • 1 replies
  • 0 kudos

LPS22 sensor suddenly behaving weird

I've had this problem with an ILPS22QS and now I'm having it with an LPS22HH. It has me completely mystified. The issue is like this: The pressure sensor works as normal for a week or even multiple weeks and then all of a sudden it enters a mode wher...

weird-behaving-pressure-sensor.png
mbenkmann by Associate II
  • 2821 Views
  • 5 replies
  • 0 kudos

AIS2120 reading issue

volatile UB__8 ubAisRxData; volatile UB__8 ubSpiStatus = 0; void SPI_vInit(void) { disable_interrupts(); configure_D_OUT_SPI_MOSI_Pin(); // PTBDD_PTBDD5 = 1; // MOSI configure_D_IN_SPI_MISO_Pin(); //PTBDD_PTBDD4 = 0; // MISO c...

IIS3DWB High-Rate FIFO/DMA Data Transfer on STEVAL-STWINBX1

Hi all, I’m working on a project using the STEVAL-STWINBX1, and my main goal is to use the IIS3DWB vibration sensor as a high-speed vibrometer. I’m still pretty new to embedded programming (about 2 months in), so please bear with me! Project setup so...

Taha by Associate
  • 1248 Views
  • 1 replies
  • 0 kudos

LSM6DSM high pass filter wake up interrupt

Hi,I am working on an accelerometer interrupt using the LSM6DSM. In AN4987 I found that I can configure the slope filter to use a window of WK_DUR samples that consecutively exceed WK_THS based on the given formula. I found good threshold settings fo...