MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LSM6DSO32 Pedometer Returns 0

Hi There, I've designed a board which uses a LSM6DSO32 sensor over i2c for accelerometer, gyro and it's embedded pedometer function. I've been able to reliably get data from the sensors accelerometer and gyro registers however I've not been able to g...

LIS2DU12 Self-Test Not Producing Expected Deviation

Hello, I’m using the LIS2DU12 accelerometer and trying to perform the positive self-test exactly as described in the official application note. However, I’m consistently seeing results that do not meet the expected deviation thresholds, and the self-...

Resolved! MSL of accelerometer sensor

Hi,Where can I find inforamtion on Moisture sensitivity level for each sensors? I checked datasheets and few other documents in the product page but couldn't find it. I want to know the MSL of IIS3DWB.Best regards,Kev

KJose.1 by Associate III
  • 716 Views
  • 1 replies
  • 1 kudos

Resolved! STM32nucleo embedded STLINK for sensortile.box

Hi, i have a question, is it possible to use the embedded STLINK on the nucleo-f446re for programming the sensortile.box (steval-mksbox1v1) ? If so, how do i have to connects the pin? I have a JTAG Adapter v1.0 (included in the sensortile box), so i'...

alemezz by Associate
  • 798 Views
  • 1 replies
  • 0 kudos

LPS22 sensor suddenly behaving weird

I've had this problem with an ILPS22QS and now I'm having it with an LPS22HH. It has me completely mystified. The issue is like this: The pressure sensor works as normal for a week or even multiple weeks and then all of a sudden it enters a mode wher...

weird-behaving-pressure-sensor.png
mbenkmann by Associate II
  • 3005 Views
  • 5 replies
  • 0 kudos

AIS2120 reading issue

volatile UB__8 ubAisRxData; volatile UB__8 ubSpiStatus = 0; void SPI_vInit(void) { disable_interrupts(); configure_D_OUT_SPI_MOSI_Pin(); // PTBDD_PTBDD5 = 1; // MOSI configure_D_IN_SPI_MISO_Pin(); //PTBDD_PTBDD4 = 0; // MISO c...

IIS3DWB High-Rate FIFO/DMA Data Transfer on STEVAL-STWINBX1

Hi all, I’m working on a project using the STEVAL-STWINBX1, and my main goal is to use the IIS3DWB vibration sensor as a high-speed vibrometer. I’m still pretty new to embedded programming (about 2 months in), so please bear with me! Project setup so...

Taha by Associate
  • 1333 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.