User Activity

this is what I see:###### AppSKey:   2B:7E:15:16:28:AE:D2:A6:AB:F7:15:88:09:CF:4F:3C###### NwkSKey:   2B:7E:15:16:28:AE:D2:A6:AB:F7:15:88:09:CF:4F:3CAT+APPSKEY=?2B:7E:15:16:28:AE:D2:A6:AB:F7:15:88:09:CF:4F:3CAT+APPSKEY=2B:7E:15:16:28:AE:D2:A6:AB:F7:1...
hello,I tried manually changing the keys from the recompiled se-identity.h file and then ran the program but the keys remain the default ones not affected by the change.how can i change them?
hello,I am using a NUCLEO-WL55JCX and I have been using the LoRaWAN_End_Node application found within the STM32Cube_FW_WL_V1.3.0 package.I would like to use the ioc file to generate a clean project and then develop a custom application.I read the rea...
I purchased a STEVAL-STWINKT1B development board and inside it has the STR485 chip for RS485 communication.I tried using the cube mx and configured it appropriately (see image 1 attached), enabled uart2, RS485 flowcontrol and then checked that the pi...
Hi,I'm working on a project where I'm supposed to save data that I collect from the XXXX accellerometer and then process it by performing an fft.I'm working on a project where I'm supposed to save data that I collect from the IIS3DWB accellerometer a...