MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Noise cancellation algorithm code.

Posted on July 27, 2014 at 17:40Hi All,My name is Gil and our company is working on a wearable electronic system.As part of our system we intend to integrate an ST digital microphone P/N: MP34DB01TR.We want to use 2 microphones in order to implement...

gil by Associate
  • 647 Views
  • 0 replies
  • 0 kudos

how to tell if the LSM330 chip is dead

Posted on June 08, 2013 at 00:27My LSM330 chip is not responding to SPI communication. Is there a way to electrically tell if the chip is dead? Thanks.

bnp979 by Associate III
  • 1096 Views
  • 1 replies
  • 0 kudos

About LPS331AP

Posted on January 10, 2014 at 07:53I am sorry that I post a question about pressure sensor at accelerometer forum, but I can't find a forum about barometric pressure sensor. I hope to know the wake up time of the chip from the power down to ready st...

hitwch by Associate II
  • 3640 Views
  • 6 replies
  • 0 kudos

Solution versus ADXL203

Posted on July 23, 2014 at 16:56I am looking for the best option versus this ADI part. Key requirements are - powered by 3.6V DC.- zero g temperature stability of 0.1 mg/C or better.- resolve angles down to 0.5 degrees at least, 0.1 degrees preferre...

PI3P on M1 module??

Posted on July 21, 2014 at 18:30I wanted too know if it is possible to use the pro version of the engine on the M1 module, is the hw compatible?Thanks for the help

franz by Associate
  • 757 Views
  • 0 replies
  • 0 kudos

H3LIS331DL 3-wire SPI

Posted on July 20, 2014 at 11:01H3LIS331DL accelerometer has 3-wire SPI mode. What i will get in this (3-wire) mode at pin number 7 (SDO in 4-wire mode). Is it pull down, pull up or open drain ?

tomasz by Associate
  • 902 Views
  • 0 replies
  • 0 kudos

Looking for EK3LV02DQ - Eval Kit software

Posted on July 19, 2014 at 15:18Transferring my life to a new machine and can't find the mini-CD that came with this eval kit.Does anyone know if it's available online and where?Thanks,Geoff #accelerometer

geoff by Associate
  • 806 Views
  • 0 replies
  • 0 kudos

Function INEMO2_SDK_Connect

Posted on June 29, 2014 at 17:20Morning, everyone,I used a demonstration board STEVAL-MKI062V2. I wrote a small C++ program and want to get data from the sensor. It looks like, that some functions are not in the dll file (''iNEMO2_SDK.dll'') .The co...

s_wd8y9x by Associate
  • 1119 Views
  • 1 replies
  • 0 kudos

LIS3DH detect position away from a zone

Posted on July 16, 2014 at 11:59Dear all,I'd like to configure the LIS3DH in order to enter my uc in sleep mode in a certain position P0 and then be awaken when the position move from P0 +/- threshold.I dont want to detect a movement but a position ...