MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! datapro 1 pack is corrupt

 Can someone please provide a working download file for "STM32Cube function pack for STEVAL-PROTEUS1 sensor datalog and file transfer over BLE and USB"?The ZIP-File Version is corrupt.It cannot be extracted neither on Windows, Linux or Mac.Thank you....

RB4 by Associate II
  • 900 Views
  • 1 replies
  • 0 kudos

Resolved! LIS2HH12 via SPI connection XYZ axis stall at fixed value

Hello.I am working with the STM32U083 and LIS2HH12TR communication via SPI. Did the SPI settings configuration in mode 3 and build a simple project in cube ide to identify and read the accelerometer data.The project also does the conversion in mg of ...

EngHwho_0-1752574142740.png
EngHwho by Associate
  • 945 Views
  • 5 replies
  • 3 kudos

Resolved! ASM330LHB Gyroscope bias changed abnormally

Hi,We are using 4 ASM330LHB in our application. We have placed 4IMU's on PCB. We put the PCB in temperature chamber to observe the sensor behaviour during the temperature variation(cooling) with 1deg/min from 30 to 60 to -20.During this test all sens...

Resolved! LIS2DUXS12 INT2 interrupt

Hello everyoneI would like to generate two different interrupts (INT1 and INT2) to detect free fall and tap.I am using MEMS studio to verify the configuration of the registers.I am using a F401RE development board with an IKS4A1 expansion that integr...

CL1 by Associate
  • 835 Views
  • 1 replies
  • 0 kudos

Resolved! If the electrode is embedded in an insulator, isn't the sensing process dielectric polarization rather than electrostatic induction?

If the electrode is embedded in an insulator, isn't the sensing process dielectric polarization rather than electrostatic induction?The following text is quoted from 「Application Note "Qvar sensing" (AN5755) p2.「 A signal is derived from the electron...

Shion by Associate II
  • 774 Views
  • 2 replies
  • 1 kudos