2023-11-19 11:11 PM - last edited on 2023-11-21 4:26 AM by Pierre SENNEQUIER
Dear,
Could you tell me if FS signal have internally pull up or pull down?
Regards
Solved! Go to Solution.
2023-11-23 6:35 AM
Hi @Stephslq ,
Welcome to ST Community!
The full scale range (2/6g or 4/12g) can be changed using the FS_4G_12G_bit in the AOFFSETOUT_Y (17h)
register. This pad has a pull-down of 30 kΩ if the PULLDOWN_FS_bit in the AOFFSETOUT_Z register is “1”, otherwise there isn’t any pull-down.
However, note that the LIS344ALH is an obsolete product, please have a look at our newest accelerometer :)
2023-11-23 6:35 AM
Hi @Stephslq ,
Welcome to ST Community!
The full scale range (2/6g or 4/12g) can be changed using the FS_4G_12G_bit in the AOFFSETOUT_Y (17h)
register. This pad has a pull-down of 30 kΩ if the PULLDOWN_FS_bit in the AOFFSETOUT_Z register is “1”, otherwise there isn’t any pull-down.
However, note that the LIS344ALH is an obsolete product, please have a look at our newest accelerometer :)
2023-11-28 12:37 PM
Hi,
You mention LIS344ALH is obsolete, do you have a direct replacement available?
Thank you
2024-12-03 10:37 AM
Which one? Could you suggest an accelerometer with the same noise level, cause lis344 is a unique one
Thank you in advance
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.