2024-11-29 7:27 AM
Hello,
I'm using the LIS2DW12 on my own board.
Consumption seems a little high to me. In the datasheet I found a value around 5.5µA and I obtained rather 45µA.The configuration is as follows:
- ODR 50Hz
- FIFO in continious mode with INT1 enabled
- Full-scale 4g
- 14 bits resolution in LP2.
I did not find any information regarding consumption in FIFO mode. Can you give me some information?
Thanks
2024-12-05 7:58 AM
Hi @laesser ,
We do not expect such high consumption. When you acquire without using FIFO what consumption do you have?