2020-11-12 2:07 AM
2020-11-12 3:56 AM
Hi @EGeor.1 ,
Well, some of these parameters are not declared in the datasheet, so I can only give an idea of typical values. For the 1.Operating temperature and 2.Storage temperature, you can refer to the datasheet, p. 14, "Absolute maximum ratings" table, last lines.
 
About the topics regarding the junction (point 4. to 7.), the LIS2DE12TR max supply is 3.6V and max current (normal mode, max ODR) is about 200uA, so the power consumed in the worst case is P=V*I=0.72mW. If you consider that the package thermal resistance is 80°C/W, the thermal difference between the device and the environment is DeltaT < 0.1°C.
Moreover, no worry about the junction temperature with respect to storage temperature.
-Eleon
2020-11-12 3:56 AM
Hi @EGeor.1 ,
Well, some of these parameters are not declared in the datasheet, so I can only give an idea of typical values. For the 1.Operating temperature and 2.Storage temperature, you can refer to the datasheet, p. 14, "Absolute maximum ratings" table, last lines.
 
About the topics regarding the junction (point 4. to 7.), the LIS2DE12TR max supply is 3.6V and max current (normal mode, max ODR) is about 200uA, so the power consumed in the worst case is P=V*I=0.72mW. If you consider that the package thermal resistance is 80°C/W, the thermal difference between the device and the environment is DeltaT < 0.1°C.
Moreover, no worry about the junction temperature with respect to storage temperature.
-Eleon
2020-11-12 4:03 AM
2020-11-12 4:27 AM
Hi @EGeor.1 ,
Which is the target application for which these data are mandatory? You can as starting point consider the overall thermal junction resistance as the previously declared 80°C/W.
-Eleon
2020-11-13 7:35 PM
2020-11-16 7:10 AM
Hi @EGeor.1 ,
The minimum and maximum Case temperature are the Storage temperature limits previously reported: the low temperature is -40°C, while the high temperature is 125°C.
On top of the Case temperature limitations, the junction temperature can vary from deltaT almost equal to zero (°C), in case the device is in power down mode and Vdd = 1.8V, to the previously calculated 0.1°C, when device is in normal mode and Vdd = 3.6V, considering the 80°C/W typical package thermal resistance.
Please note that the thermal behavior of the device can be influenced by the environment, if for example it is soldered near the application processor or other heat-generating components.
-Eleon