User Activity

We have configured TIM2 Channel 1 to capture rising edge on PA0 pin.We have enabled DMA1 Stream5 to read data on Port D and copy to local array.The callback function for DMA1 is not triggered.Please let us know, if we are missing any configuration.No...
We have designed custom board which has STM32F446RE MCU and ISM330DLC vibration sensor.We are able to send FFT data with 512 sample to Unicleo-GUI and able to observe the FFT data for X,Y,Z axis on graph.But when we send FFT data with 1024 samples t...
Hi,We are using ISM330DLC MEMS sensor in our project and trying to interface sensor using X-CUBE-MEMS1 library. In configuration parameters, SPI module is not visible. Please suggest how to configure X-CUBE-MEMS1 library to interface using SPI module...
We are able to run the TouchGFX code on target using TouchGFX 4.15.0 version.When trying to port the generated to custom project created using STM32CubeIDE 1.4.2 version the display does not work.I request correct configuration setting for display on...
We are using X-Nucleo-IKS02A1 board to test the vibration sensor using vibration monitoring example code. The FFT data of vibration sensor is observed using Unicleo-GUI.It is observed that the FFT data is not represented in Unicleo-GUI when FFT size ...