2020-11-10 12:00 AM
Hi all,
I opened a issue on github about it:
https://github.com/STMicroelectronics/STMems_Android_Sensor_HAL_IIO/issues/6
Once i add the STMems_Android_Sensor_HAL_IIO library on my system the sensor service crash.
01-01 00:02:12.558 2358 2358 F DEBUG : Revision: '0'
01-01 00:02:12.558 2358 2358 F DEBUG : ABI: 'arm'
01-01 00:02:12.558 2358 2358 F DEBUG : pid: 2355, tid: 2355, name: android.hardwar >>> /vendor/bin/hw/android.hardware.sensors@1.0-service <<<
01-01 00:02:12.558 2358 2358 F DEBUG : signal 11 (SIGSEGV), code 1 (SEGV_MAPERR), fault addr 0x1c
01-01 00:02:12.558 2358 2358 F DEBUG : Cause: null pointer dereference
01-01 00:02:12.559 2358 2358 F DEBUG : r0 00000001 r1 00000000 r2 af5905c8 r3 00000000
01-01 00:02:12.559 2358 2358 F DEBUG : r4 af5905c8 r5 0000005a r6 00000000 r7 00000003
01-01 00:02:12.559 2358 2358 F DEBUG : r8 bebad354 r9 00000004 sl 00000000 fp bebab950
01-01 00:02:12.559 2358 2358 F DEBUG : ip af86062c sp bebab910 lr af8252ad pc af371b64 cpsr 200e0030
01-01 00:02:12.619 2358 2358 F DEBUG :
01-01 00:02:12.619 2358 2358 F DEBUG : backtrace:
01-01 00:02:12.620 2358 2358 F DEBUG : #00 pc 00007b64 /vendor/lib/hw/STsensors.msm8909.so (st_hal_open_sensors(hw_module_t const*, char const*, hw_device_t**)+275)I don't know if this is the official way to report a bug, Otherwise let me know the right way to do it.
Thank you in advance.
Solved! Go to Solution.
2020-11-10 7:47 AM
Hi @DevM ,
you are right, the official way to open an issue concerning those Android libraries is reporting it on Github.
Same for the C libraries, for example.
Please let me know if you will or will not receive a feedback (in about 1 week max).
Edit: the topic should now be closed on Github.
-Eleon
2020-11-10 7:47 AM
Hi @DevM ,
you are right, the official way to open an issue concerning those Android libraries is reporting it on Github.
Same for the C libraries, for example.
Please let me know if you will or will not receive a feedback (in about 1 week max).
Edit: the topic should now be closed on Github.
-Eleon
2020-11-16 2:33 AM
Hi @Eleon BORLINI ,
Any update on the issue?
Thank you.
2020-11-16 3:18 AM
Hi @DevM ,
uhm... let me please check internally and then come back to you.
-Eleon