MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! LSM6DSV on STEVAL MKI239A with Nucleo board via SPI not working

helloI've been trying to use the LSM6DSV on it's steval-mki239a board with a nucleo board (nucleo-l476rg) via SPI and the lsm6dsv is not answering whatever the configuration of my SPI is.The sensor is fine since it work with the steval-mki109v3 board...

Eddess_0-1743493087888.png Eddess_1-1743495078971.png Eddess_2-1743495176541.png Eddess_5-1743495442778.png
Eddess by Associate II
  • 463 Views
  • 1 replies
  • 1 kudos

LIS2DH12 HOWTO Convert Register value to mg value

Hi,  I am using the LIS2DH12 to interrupt me on an inertial wake.  I am running in Low Power mode with a scale of 4G.  After verifying that the X axis produced the force that caused the interrupt I read the X_OUT_L and X_OUT_H registers to get the 2'...

DPatt.2 by Associate II
  • 731 Views
  • 4 replies
  • 2 kudos

Lis3dh reading not repeatable/stable

HiWe are developing a project in which we are using LIS3DH to calculate the angle and based on that angle we stop/start an actuator.The sensor is mounted on a PCB which is aligned along x axis i.e. when stationary the acceleration in x axis is 1g * 9...

lis3dh.png
pthakkar by Associate II
  • 491 Views
  • 2 replies
  • 0 kudos

Resolved! LPF2 on IIS3DWB and anti-alias

I use IIS3DWB with no LPF2 enabled, and I understand the Frequency response shown in Figure 13 at page 20 of the datasheet.I know that I can enable low-pass LPF2 filter, but from the same graph I don't understand if this filter can be enabled as a ha...

vix by Associate II
  • 2321 Views
  • 6 replies
  • 0 kudos