LSM6DSV on STEVAL MKI239A with Nucleo board via SPI not working
- April 1, 2025
- 1 reply
- 992 views
hello
I've been trying to use the LSM6DSV on it's steval-mki239a board with a nucleo board (nucleo-l476rg) via SPI and the lsm6dsv is not answering whatever the configuration of my SPI is.
The sensor is fine since it work with the steval-mki109v3 board ans the MEMS studio
I checked the SPI signal on the steval mki109v3 with a logical analyzer and found several odd things but the sensor is answering

I don't know if it is my analyzer but the MISO line is always stuck at 1 and the level of MOSI are strange but the sensor understand the message and answer with the right value (WHO_AM_I register: MOSI should send 0x0F and MISO answer 0x70)
On the other end I tried to recreate the same configuration on my nucleo board but the sensor doesn't answer any command
I tried:
full duplex master CPOL=1 CPHA=1


with external pull up on MISO

full duplex master CPOL=1 CPHA=0

with external pull up on MISO

I tried in master half duplex


with external pull up on MISO

I tried master half duplex with CPHA =0 (1 edge)

with external pull up on MISO

I've been trying to make this work for more than a week now and tried all possible configuration but nothing works. what could be wrong? did I miss something?
I'm using the LSM6DSV library found here https://github.com/STMicroelectronics/lsm6dsv-pid/tree/7b98628713090244cf14f54d9059938cb00342fd that I adapted following the readme file
I attached my complete project