MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! MEMS Studio Not Detecting STEVAL-MKI109D

I followed 'STEVAL-MKI109D Professional MEMS Tool motherboard for MEMS adapter boards' and installed MEMS Studio.I then placed STEVAL-MKI250KA on STEVAL-MKI109D by following UM3420 and AN6173.  When I boot MEMS Studio, it just does not recognise the ...

no conn.png
seanjm by Associate
  • 505 Views
  • 1 replies
  • 1 kudos

Resolved! Query about MDRDY Signal Configuration in LSM6DSO16IS MODE2

I am working with the LSM6DSO16IS in MODE2 configuration with ISPU enabled. I have some questions regarding the MDRDY (Master Data Ready) signal:1. How is the MDRDY signal handled in MODE2 when using the master I2C interface with external sensors?2. ...

seanfan by Associate
  • 430 Views
  • 1 replies
  • 0 kudos

Unable to read the mic value IMP34DT05TR

We are interfacing the IMP34DT05TR microphone with the STM32F423ZHJ6 microcontroller. I have attached the schematic for reference. However, we are unable to read the microphone data on our custom board, as we always get a NULL value in the output. La...

srinithi_09_0-1743055976941.png

Stream sensortile box pro data via USB into Matlab

Hello, I have the sensortile box pro. I have used the algobuilder in the MEMS-studio to configure various data outputs (Acc, Gyr, RotationVector 6x). The sensortile isplugged in with USB. I can see those data coming into the MEMS-studio algobuilder e...

Gawa by Associate
  • 502 Views
  • 2 replies
  • 2 kudos

Problem with Heading Calculation

I'm using ST MotionFX v2.7.1 and have encountered an issue with heading calculation.I'm following the sample code from the document:um2220-getting-started-with-motionfx-sensor-fusion-library-in-xcubemems1-expansion-for-stm32cube-stmicroelectronics #d...

gtk by Associate
  • 450 Views
  • 2 replies
  • 1 kudos

LSM6DSV: Z acceleration values too high by 1g

Hi,I read the LSM6DSV on the STEVAL SMKI239AA using a Raspberry Pi Pico running Circuit Python. The CTRL1 register is set to 0x07 (240 Hz ODR, high performance). My output is converted to m/s^2 and looks like that when I move the sensor board slowly:...

PeterK by Associate II
  • 499 Views
  • 3 replies
  • 0 kudos

LPS22HH absolute accuracy

Helloin the data sheet of LPS22HH the absolute accuracy is  ±0.5 in which range of pressure ? ( 800 hPa to 1100 hPa) ? because i tested some samples in 0.3 bar and 0.5 bar, there big difference between the mesure of LPS22HH and reference (exactly val...

ljm by Associate III
  • 519 Views
  • 1 replies
  • 0 kudos

Resolved! how to use motionfxi

I want to use the motionfx library in the x cube mems1 package for my flight control card and ahrs project, my aim is to obtain roll pitch and yaw values with sensor fusion, but I have not come across an example code for using motionfx. Can anyone he...