Skip to main content
Soundhar
Associate II
November 11, 2022
Question

How to set LSM6DSM in 3-wire SPI mode with C standard MEMS library

  • November 11, 2022
  • 3 replies
  • 2020 views

I have recently brought a STEVAL-STLKT01V1 SensorTile kit in which LSM6DSM, LSM303AGR & LPS22HB are connected in 3 wire SPI on the SPI2 line of STM32L476. I pulled 4 CS lines to high at the beginning of the program and have set the SPI2 to Half duplex master mode with low data transfer rate. even though using the c command  lsm6dsm_spi_mode_set(&dev_ctx, LSM6DSM_AUX_SPI_3_WIRE); I'm getting no response on spi read, so the program is getting struck at lsm6dsm_reset_get(&dev_ctx, &rst).

 

I was able to use 4 wire SPI with STM32F407 and LSM6DSM, but I still face issues with using 3 Wire mode with STM32F407 and LSM6DSM

 

i have defined the CS Pin:

 

#define CS_up_GPIO_Port CS_AG_GPIO_Port

#define CS_up_Pin CS_AG_Pin

 

my GPIO Configuration:

 

 

 

Sensor Initialization:

 

/* Initialize mems driver interface */

 stmdev_ctx_t dev_ctx;

 dev_ctx.write_reg = platform_write;

 dev_ctx.read_reg = platform_read;

 dev_ctx.handle = &SENSOR_BUS;

 

 /* Wait sensor boot time */

 HAL_Delay(15);

 

 lsm6dsm_spi_mode_set(&dev_ctx, LSM6DSM_AUX_SPI_3_WIRE);

 lsm6dsm_auto_increment_set(&dev_ctx, 1);

 

 /* Restore default configuration */

 

 lsm6dsm_reset_set(&dev_ctx, PROPERTY_ENABLE);

 do {

  lsm6dsm_reset_get(&dev_ctx, &rst);

 } while (rst);

 

 /* Enable Block Data Update */

 lsm6dsm_block_data_update_set(&dev_ctx, PROPERTY_ENABLE);

 

 /* Set Output Data Rate for Acc and Gyro */

 lsm6dsm_xl_data_rate_set(&dev_ctx, LSM6DSM_XL_ODR_12Hz5);

 lsm6dsm_gy_data_rate_set(&dev_ctx, LSM6DSM_GY_ODR_12Hz5);

 

 /* Set full scale */

 lsm6dsm_xl_full_scale_set(&dev_ctx, LSM6DSM_2g);

 lsm6dsm_gy_full_scale_set(&dev_ctx, LSM6DSM_2000dps);

 

 /* Configure filtering chain(No aux interface)

  * Accelerometer - analog filter

  */

 lsm6dsm_xl_filter_analog_set(&dev_ctx, LSM6DSM_XL_ANA_BW_400Hz);

 

 /* Accelerometer - LPF1 path (LPF2 not used) */

 //lsm6dsm_xl_lp1_bandwidth_set(&dev_ctx, LSM6DSM_XL_LP1_ODR_DIV_4);

 

 /* Accelerometer - LPF1 + LPF2 path */

 lsm6dsm_xl_lp2_bandwidth_set(&dev_ctx, LSM6DSM_XL_LOW_NOISE_LP_ODR_DIV_100);

 

 /* Accelerometer - High Pass / Slope path */

 //lsm6dsm_xl_reference_mode_set(&dev_ctx, PROPERTY_DISABLE);

 //lsm6dsm_xl_hp_bandwidth_set(&dev_ctx, LSM6DSM_XL_HP_ODR_DIV_100);

 

 /* Gyroscope - filtering chain */

 lsm6dsm_gy_band_pass_set(&dev_ctx, LSM6DSM_HP_260mHz_LP1_STRONG);

 

SPI Read & Write:

 

static int32_t platform_write(void *handle, uint8_t reg,

               uint8_t *bufp,

               uint16_t len)

{

 

  HAL_GPIO_WritePin(CS_up_GPIO_Port, CS_up_Pin, GPIO_PIN_RESET);

  HAL_SPI_Transmit(handle, &reg, 1, 1000);

  HAL_SPI_Transmit(handle, bufp, len, 1000);

  HAL_GPIO_WritePin(CS_up_GPIO_Port, CS_up_Pin, GPIO_PIN_SET);

 

}

 

static int32_t platform_read(void *handle, uint8_t reg, uint8_t *bufp,

              uint16_t len)

{

 

  reg |= 0x80;

  HAL_GPIO_WritePin(CS_up_GPIO_Port, CS_up_Pin, GPIO_PIN_RESET);

  HAL_SPI_Transmit(handle, &reg, 1, 1000);

  HAL_SPI_Receive(handle, bufp, len, 1000);

  HAL_GPIO_WritePin(CS_up_GPIO_Port, CS_up_Pin, GPIO_PIN_SET);

 

}

 

kindly reply what's the issue with the above-followed procedure

This topic has been closed for replies.

3 replies

ABayl.2
Associate
December 27, 2022

Hi @Soundhar​ . Can you solved the problem ?

Visitor II
October 7, 2024

Hi,

Can you solved the problem? Because I have know the same problem.

Visitor II
March 31, 2025

Same problem but on 4 wire mode i can read id but stuck at reset