2025-03-25 5:40 PM
Anyone have any idea if the temperature can remain the same for long periods of time in a stable environment?
2025-03-27 7:25 AM
Hi @hmckee ,
It should. Did you try?
2025-03-27 2:23 PM
Yes, that's the issue. We've set up our device so that it marks the LPS22 in error if it reads the same value 45 times in a 30 min period. The condition has occurred in both a stable, temperature controlled environment and in an uncontrolled environment.
The purpose of this was to determine if the LPS22 is functioning properly. Maybe this is an unrealistic expectation.