Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.
Hello everyone,We have successfully setup MotionMC lib in our project in order to calibrate the magnometer embedded in the MPU9250 IMU chip. When the board is turned on, after 15-45 sec (depending on rotating the board), MotionMC calculates the soft&...
Hello Community,I am working on a machine learning project and I am using an accelerometer sensor "STEVAL-MKI190v1". The board description and documentation can be found on this link The driver files for it is available on this github link. Now I hav...
The current script in BlueSTSDK examples (https://github.com/STMicroelectronics/BlueSTSDK_Python) needs to be run as root to scan for bluetooth devices in the vicinity. Question is if it is possible to connect to a bluetooth device and receive data w...
Hi, I'm using the STEVAL-STWINKT1B development board to read the iis3dwb accellerometer and write to the sd as in the HSdatalog example.To do this I use freertos and fatfs.I created the project first on CubeMx where I set the parameters to read SPI, ...
Hardware: SensorTile.boxThe project readme.txt file suggests that the software should start from the memory address 0x08004000 in FLASH. How can I change this when I am downloading the software from the Android app? The board has to be restarted aft...
Can someone please tell me the sequence and list of registers / bits I need to touch to get this device into 3 wire SPI mode?....I am monitoring it on a logic analyzer and continue to see the data from the device on the MISO line....I am running at 4...
Hello experts,I'm trying to determine if the ASM330LHH IMU can eliminate false positives by itself or if the MCU will need to address them. I've searched the forum for this topic and didn't find anything specifically related to this device. Apologies...
Dear @Imen DAHMEN ,Is there any plan to have the PDM2PCM library in the Middleware for STM32WL microcontrollers?Thank you much.