MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! IIS3DWB Interrupt stops triggering while sampling for long periods

I have been using the IIS3DWB evaluation board alongside TIs CC1352P2 uC to bring up software ahead of the actual hardware arriving. The SPI bus speed is 8MHz in mode 3.The IIS3DWB is configured only sample accelerometer data on 3 axis and to store t...

0693W000007Dqr6QAC.jpg 0693W000007DqrLQAS.jpg
JDoug.1 by Associate II
  • 6354 Views
  • 10 replies
  • 0 kudos

Resolved! Unico-GUI tools bar - icons showing up on top of each other

Well, the Unico-GUI software was working fine, and one day all of the tools (bars, plot, data, etc) started getting drawn on top of one another, and the last one (pedometer) is the one on "top" and the only one I can now select. Any idea how to fix ...

0693W00000SucYeQAJ.png
Brian Rau by Associate III
  • 1718 Views
  • 3 replies
  • 0 kudos

LSM6DS0X STEP COUNT READ BUG

After loading a new decission tree for the Machine Learning Core the behaviour of the Step count registers of the pedometer changed.I must note that none of the code changed, just the register mapping corresponding the decision tree loaded to the MLC...

PPill.1 by Associate
  • 1121 Views
  • 1 replies
  • 0 kudos

LSM6DSO32 taking High Current

I have powered from LSM6DSO32 through a 3V Coin cell battery and connected with Nrf52810 using I2C.Without any coding sensor taking around 2mA and after flashing its taking 4MA.I am getting the readings correctly.Attached the schematics

0693W00000SttviQAB.png
V.Jose by Associate II
  • 1790 Views
  • 3 replies
  • 0 kudos

Step count is non-zero even though object is stationary (LIS2DS12)

Hello ST,I am using LIS2DS12 sensor for step detection application. I read the step count register every 1 minute and reset the count value. I observe that even if the object is stationary, the step count register has a non-zero value (The value vari...

AB.4 by Associate II
  • 2320 Views
  • 5 replies
  • 0 kudos

LSM6DSxx Gyro "Ringing"

I'm trying to use several different IMUs in the LSM6DS family (LSM6DSOX and LSM6DSO32). Both of them are exhibiting "ringing" on the three gyro axes when exposed to shock (knocking the PCB against a table). It almost looks like there's no anti-aliasi...

JimJ by Associate
  • 1649 Views
  • 1 replies
  • 0 kudos