cancel
Showing results for 
Search instead for 
Did you mean: 

Hi, We have STEVAL-MKI159V1. We need to test the features like (Accelerometer, Gyroscope, Magnetometer) data with provided MEMS1 library. Can anyone please suggest required board that can integrate STEVAL-MKI159V1 directly to read data (Acc,Gyro,Mag)?

VB.4
Associate II
 
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Peter BENSCH
ST Employee

Welcome, @Community member​, to the community!

on the website of the STEVAL-MKI159V1 you will find the reference to the motherboards STEVAL-MKI109V2 and the  STEVAL-MKI109V3.

Please note that STEVAL-MKI109V2 is no longer recommended for new designs (NRND).

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
VB.4
Associate II

Thank you for the reply @Peter BENSCH​,

I've referred the boards you suggested. But thing is can we use those boards for development also.? As per my knowledge those boards doesn't support for

development only for data monitoring. Also studied that we have to use those boards with ARM Cortex M series Eval boards. So please confirm me on the board that supports data monitoring as well as development. Requirement is we need to read Acc, Gyro, Mag data directly from  STEVAL-MKI159V1 and use those data for development without any middle boards like "motherboards". Can we interface STEVAL-MKI159V1 directly to dev board to test & develop ?

Any help would be very thankful.

The adapter boards should enable the fastest possible evaluation of the respective sensor, for which an mcu is needed. In order to avoid having to provide a complete board with mcu for each sensor, the sensors are assembled on an adapter board that can be quickly plugged onto a motherboard, for example.

These adapter boards can also be connected to any other microcontroller. They are also intended for data monitoring in the context of a development, but not for productive use in a finished device, as you can read in the Evaluation Board Terms Of Use:

The Evaluation Board offers limited features and is conceived to be used only to evaluate and test ST products in a research and development setting. 

[...]

The Evaluation Board shall not be, in any case, directly or indirectly assembled as a part in any production of Yours as it is solelydeveloped to serve evaluation and testing purposes and has no direct function and is not a finished product.

If the Evaluation Board is incorporated in an evaluation system, the evaluation system may be used by You solely for Your evaluation and testing purposes. Such evaluation system may not be offered for sale or lease or sold, leased or otherwise distributed for commercial purposes and must be accompanied by a conspicuous notice as follows: “This device is not, and may not be, offered for sale or lease, or sold or leased or otherwise distributed for commercial purposes�?.

Does it answer your questions?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.