User Activity

Hi Team,I searched sensor fusion performance information of LSM9DS1TR, LSM6DSO IMUs as below,1. Static Accuracy (Yaw, Pitch, Roll) = ?2. Dynamic Accuracy (Yaw, Pitch, Roll) = ?3. Orientation Settling time = sec?However, I did not find it in the respe...
Hi Team,We are working on BHI160B BOSCH IMU sensor using STM32L053R8 board. We can read the Quaternions, calculate RPY. But now we are finding a Yaw drift issue with that IMU. Could an expert from ST help us solve this technical issue?Also, Is there ...
I'm using STM32-NucleoL053R8 board. I'm Getting error when I build my project I have included required libraries and its path to the project still getting error. I tried with the manual method like adding lib to the "MotionAC2_CM0P_wc32_ot.a" file ad...