Resolved! Marking code
Hi ST Team,Can you share the Marking code specification for the product: LPS22DFTR ?Thanks, Danny.
Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.
Hi ST Team,Can you share the Marking code specification for the product: LPS22DFTR ?Thanks, Danny.
I'm using the LSM6DSOX which can measure ±2000dps and ±16g for each axis with the correct settings. I'm wondering if there is a reliable way to detect if the motion of the sensor went beyond those limits during a given time window. Does the sensor re...
Hello,We are using the LIS2DH12TR sensor in our project. As per the datasheet, I understand that it always shows +1g on the +Z-axis when the IC is at rest.We are operating the sensor in HR mode under different modes 2g, 4g, 8g and also in 16g mode. ...
Hello,I am using a LSM6DSO32 on a custom board. As an attempt to save power in sleep mode we want to place the device in ULP (ultra low power mode) as specified by the datasheet. I have attached my function that initializes the device in ULP mode a...
Hello. I made all the adjustments for my STEVAL kit. I also installed the necessary binary file in the Wifi module (Dsh predmnt). According to the guide I gave in the link, I stay on page 12 step 8. When I enter the wifi id password, it does not conn...
Hi Everyone, Below Linux driver for LSM6DSL device has no method to read the temperature sensor. https://elixir.bootlin.com/linux/latest/source/drivers/iio/imu/st_lsm6dsxIs there a complete Linux driver which reads the temperature as well?thanks,
Hi,I have two LPS28DFW in my application. The absolute value as well as the difference is important here. I noticed that there is a difference of around 30 Pa. Is it reasonable to assume that this difference is roughly constant in the future? I teste...
Hi! I hope somebody can help me. I am trying to get the sensory_tnl example of the X-Cube-LocalVUI package on the STM32H747I-DISCO with the STEVAL$MIC008AA (dual MEMS Microphones) board working. Unfortunately, I cannot get any audio signals although ...
Hi!We are a group trying to get reliable rotation data out of the LSM6DSV16X sensor. The accumulated error values in the datasheet seemed promising. However, we are currently in a state, where the sensor is returning gyroscope data, but the actual ob...
Greetings,I have been trying to read the sensors from the ISM330DLC using its FIFO. However, when reading the number of samples (FIFO_STATUS1/2), it remains 0 with just dataset 1 and 2 enabled. When enabling dataset 4 with either, or and temperature ...