MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Asm330 low frequency behavior

Hi I have a questionI am using asm330lhh gyroscopeThe sensor is great but I see some kind of low frequency behavior in the data from this sensorMy ODR is 6667 range is 500The accuracy is good, but this low frequency behavior will eventually cause pro...

image_20230804_231800a997c2ca-dcd2-4cf8-aac5-0027bd9d4e55.jpg image_20230804_231805a044cff2-b268-48bb-a6d7-c22c7c3f092e.jpg
AHass.5 by Associate II
  • 2062 Views
  • 3 replies
  • 0 kudos

ASM330LHB-Query

 Dear team,I'm using ASM330LHB for Electronics Brake control project.Please clarify my queries to use this ASIC in our application.How the ASIC is claimed as ASIL-B? Is there any redundancy in the ASIC itself?How the error detection and error reactio...

ganand05 by Associate
  • 1684 Views
  • 2 replies
  • 0 kudos

pdm2pcm, pcm data noisy , pdm mic nucleo f413zh

hello tout le monde, im worknig on audio project im trying to get data from a pdm microphone as pcm 8 bit and transmit the data via uart  as binary but when i transfer the data from binary to audio via audacity i can hear just noise nothing else, als...

zohbou1 by Associate
  • 2217 Views
  • 1 replies
  • 0 kudos

Resolved! Strange noise distribution for gyro data from LSM6DSOX

When looking at a chart of integrated single-axis gyro data with a completely stationary sensor, I noticed that there are fairly large jumps once in a while.Since this doesn't look like brownian motion with normally distributed steps, I plotted a his...

imu-integration-chart.png raw_hist.png

Resolved! Difference between each mode of pedometer in LSM6DSOX

Hi,I am implementing the pedometer function using LSM6DSOX.According to the driver file provided by ST, there are three different modes to configure. I want to know the difference between them. I cannot find any information in the datasheet.Appreciat...

Jiabin_0-1690953853420.png
Jiabin by Associate II
  • 4156 Views
  • 8 replies
  • 5 kudos

bring up sensors on steval-mki128v6

Hi,When bring up sensors on steval-mki128v6,  for accelerometer and gyro,  read out who_am_i value is 0x6A, which means lsm6dsm. I can use user application to get samples. But I can't find any steval-mki128v6 document online.V5 is lsm6ds3, V7 is lsm6...

lola by Associate
  • 1390 Views
  • 1 replies
  • 0 kudos

IMU sensor LSM6DSV FIFO Timestamp drift

We are observing that LSM6DSV FIFO Timestamp is drifting at a constant rate when Gyro sensor is enabled.Our ImplementationWe are using 6-axis IMU sensor LSM6DSV with st_lsm6dsvx driver from ST GitHub and integrated with OSD32MP157 SiP.We've modified ...

sw_clock _Screenshot 2023-06-14 at 1.18.28 PM.png hw_clock_image.png
farid by Associate II
  • 3858 Views
  • 1 replies
  • 0 kudos

Calculating Analog reference voltage using vref macro

I am using stm32wl55 controller to Calculate Analog reference voltage using vref macro, which is defined as follows:#define __HAL_ADC_CALC_VREFANALOG_VOLTAGE(__VREFINT_ADC_DATA__,\                                          __ADC_RESOLUTION__) \__LL_AD...

Aanchal by Associate II
  • 2481 Views
  • 0 replies
  • 0 kudos