User Activity

Hello guys,i have checked stm cases for predictive maintanence (https://stm32ai.st.com/use-cases/applications-predictive-maintenance/), and i realised that most of solutions are made for industrial. I want to make predictive maintenance for product, ...
I have STEVAL-MKI208V1K but not its own compatible motherboard. I want to use IIS3DWB sensor. When i connec SDA, SCL, GND and VDD(for vdd i have tried 3v3 and 5v), HAL_OK said HAL_ERROR. Is this STEVAL-MKI208V1K can be used standalone or no? Thanks f...
i have B-G431B-ESC1 board and motor. I can not profile this motor. X-CUBE-MCSDK-6 have issue that when i wrote max speed for example 30 000, my motor is go up to 3 000 which is 10% of max. In order to solve this issue i am using X-CUBE-MCSDK (version...
Hello I have STEVAL-STWINKT1B device. When i try to connect wifi with tera term it gives this error:platform_init L#234 The network interface can not be startedany advice?
Hello. I made all the adjustments for my STEVAL kit. I also installed the necessary binary file in the Wifi module (Dsh predmnt). According to the guide I gave in the link, I stay on page 12 step 8. When I enter the wifi id password, it does not conn...
Kudos given to