User Activity

Hi,Thanks for your help in advance.I have a custom Linux board with a lsm6dsl module on the platform. The driver has been ported and I can read the Accelerometer and Gyro raw data from the Linux usersapce sysfs file entries. an interrupt line from th...
Hi all,I Have a custom board that runs Linux. The board has a LSM6DSL module on it as well. the IMU driver has been ported into the Linux Kernel and I have access to the Accelerometer output registers from the Linux  sysfs entries under  /sys/bus/iio...
Hi Everyone, Below Linux driver for LSM6DSL device has no method to read the temperature sensor. https://elixir.bootlin.com/linux/latest/source/drivers/iio/imu/st_lsm6dsxIs there a complete Linux driver which reads the temperature as well?thanks,   
Hi, I am experimenting with STEVAL-ID008V2 evaluation board and the DTM project from the SDK. It seems the DTM firmware using the external 32KHz clock for as the Low frequency clock source. Where about the source code of the DTM project I could set t...
I need a DTM firmware for BlueNRG2 which works wirelessly with the equipment shown in the image. I wonder if ST provides their customers with such a firmware? thanks,
Kudos given to