MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STEVAL MKI109V3 does not recognize other STEVAL adapters

HI,My MKI 109V3, even after firmware update, does not recognise adapters MKI197V1 or MKI212V1 (The WHO_AM_I register value does not match the device selected).I tried on two different laptops with windows 10.What am I doing wrong?thank you in advance...

AngeloB by Associate II
  • 3924 Views
  • 4 replies
  • 0 kudos

Resolved! STEVAL-MKI168V1 with IIS2DH I2C issues

HiI currently try to integrate the STEVAL-MKI168V1 for a development board via I2C.I use a TI MCU and use the default drivers provided by ST. The sensor does not respond to the defined I2C addresses of 0x31 resp. 0x33 if SA0=1. After doing a I2C scan...

LSM6DS3 Gyroscope anti-aliasing filter configuration

Hi everyone,I am using an LSM6DS3 IMU sensor for my current project.In Application Note AN4650, I read that the gyroscope analog signal coming from the mechanical parts is filtered by a low-pass anti-aliasing filter (having a constant bandwidth). Do ...

Resolved! STEVAL-MKI218V1 + Nucleo F401RE I2C communication

Hi,I am on a steep learning curve here. There are huge gaps in my understanding of the field, so any help will be most appreciated. Basically I am trying to connect to AIS2ih accelerometer (on Steval-mki218v1) with my Nucleo board, and try to communi...

LSM6DS3TR-C not detected via adafruit library

I recently bought LSM6DS3TR-C sensor from local market. I tried to measure the accelerometer using Adafruit_LSM6DS and SparkFun_LSM6DS3_Arduino_Library library. In both case the sensor was not recognized. I found the sensor was working. It responded ...

WhatsApp Image 2023-08-10 at 8.32.06 PM.jpeg WhatsApp Image 2023-08-10 at 8.32.07 PM.jpeg

Can i use STEVAL-MKI208V1K standalone ?

I have STEVAL-MKI208V1K but not its own compatible motherboard. I want to use IIS3DWB sensor. When i connec SDA, SCL, GND and VDD(for vdd i have tried 3v3 and 5v), HAL_OK said HAL_ERROR. Is this STEVAL-MKI208V1K can be used standalone or no? Thanks f...

bcryhun by Associate II
  • 1105 Views
  • 1 replies
  • 0 kudos

IIS2MDC

Hi,My thesis topic is to develop a dynamic preventive maintenance schedule for medical devices based on their usage. For this purpose, I have been collecting data using a magnetometer sensor (, we use IIS2MDC) 24/7 for the past 3 months. I need guida...

ABulu.2 by Associate II
  • 1502 Views
  • 1 replies
  • 0 kudos

Resolved! ST sensor - LPS27HHTW pressure read out problem

I would like to read out the pressure reading from this sensor, but it keep returning '0' Status.Tools: Nucleo-767ZI, STM32CUBEIDE, STEVAL-220VI (the sensor eval)I connect Sensor VDD to 3.3V,CS pin to VDD_IO,SDA, SCL pulled up by 4kOhm to 3.3V,INT/DR...

Wai Siang by Associate III
  • 3841 Views
  • 6 replies
  • 3 kudos