MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Impedance of the SDO - ASM330LHH

Hi,What is the output impedance of the SDO pin?I'm doing a schematic with this components and I want to match the impedance of the trace. Thank you.

fposser by Associate III
  • 1011 Views
  • 0 replies
  • 0 kudos

Enable vibrometer in STWINKT1B

Hello Everyone,In STWINKT1B, I need to enable the IIS3ZDWB sensor (vibrometer) and should be able to measure vibration of the given object with my phone via Bluetooth but the ST BLE Sensor Classic app is only showing the environmental parameters.Can ...

PD by Associate
  • 945 Views
  • 1 replies
  • 1 kudos

Resolved! STWINKT1B STREAMING USB

Hi,I bought the STEVAL-STWINKT1B hoping to be able to store and plot real-time data from my accelerometer, both in the time domain and in the frequency domain (performing FFT) for the purpose of developing my project. I bought it thinking that it wou...

Vibration sensor sleep mode

Hi,We confirmed that it is due to vibration sensor (IIS3DWBTR) only because when we removed sensor IC and tested remaining board the consumption was 7.4uA with micro controller (STM32) , memory also. But after placing vibration sensor and making it i...

LIS2DH12 accelerometer values suddenly close to zero (-4, 0, 4)

Posted on November 14, 2017 at 21:08Dear allWe are using LIS2DH12 accelerometer in our product. We are juat about to launch the production and sales when we faces a weird problem.Suddenly the accelerometer starts reporting values like 0, 4 and -4, i...

Resolved! How to display the float value in Cube IDE .

 I am using Sprintf, but I cant see the number in UART LPS22HH_pressure=LPS22HH_GetPressure();   sprintf(result,"%4.2f", LPS22HH_pressure); // @suppress("Float formatting support")I have also tried %g

IIS3DWB uses ~275uA in Low power mode - not 5uA-16uA

I have an issue with current consumption of a IIS3DWB using the STEVAL-MKI208V1 kit.I have previously discussed it in this issue, but I've traced (i hope) the issue to the VDDIO pin.I'm using a STM32WB55CEU6 as SPI master.To measure current I'm using...

0693W00000QKYsGQAX.jpg 0693W00000QKYsLQAX.jpg 0693W00000QKYsBQAX.jpg 0693W00000Nt7M1QAJ.png
KMeld.1 by Associate III
  • 2385 Views
  • 4 replies
  • 0 kudos

Resolved! LSM303AH -1G/1G Unexpected Output, Less than 90 degrees

Hello,I am having issues with my acceleration data being output from my LSM303AHTR. I have configured it for 2G Full scale making the "sensitivity" 0.061mg/lsb.I have tested two LSM303AH chips on two of our custom PCBs. I am getting similar results o...

wb346 by Associate II
  • 3833 Views
  • 10 replies
  • 2 kudos

IIS2DH FIFO stream mode configuration issues

HiI am using an IIS2DH accelerometer and set up FIFO. The configuration sequences are following the IIS2DH example in Github, see below// 25Hz, Low-Power Mode Disabled, XYZ enabledACC_Write_Command(IIS_CTRL_REG1, IIS_CTRL_REG1_INIT_25HZ);// High-Pass...