MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! LIS3DSH, SDO Pullup Register

Hello,We have been using the LIS3DH for some time and recently acquire some LIS3DSH' as well.With both modules there is an internal pull-up for the SDO pin, and with the LIS3DH there is a register to control this pullup:CTRL_REG0I am not able to find...

videojames_0-1695096274516.png

Resolved! FSM compatibility with SFLP or tap detect in LSM6DSV?

I have four FSM programs working with the LSM6DSV sensor, all set to AODR/GODR of 30Hz in line with the examples I copied. Tap detect requires significantly higher ODR.  I might also want to run the SFLP at a rate higher than 15 or 30 Hz, so does thi...

KWine by Senior
  • 2321 Views
  • 3 replies
  • 0 kudos

LIS3MDL hard iron offset registers

 Hi, the datasheet for the LIS3ML does not mention any dedicated offset registers that can be used to deduct an offset vector from the measurements: However, when I view the LIS3MDL app note, it says they are there: The app note points to 05h through...

Schermafbeelding 2023-10-16 om 14.59.54.png Schermafbeelding 2023-10-16 om 15.01.33.png

Resolved! LSM6DSV16X chip does not work.

LSM6DSV16X chip does not work.I purchased the LSM6DSV16XTR chip, then looked at the datasheet and built a simple circuit.But SPI communication doesn't work.I used the LSM6DSV16X arduino library provided by Sparkfun, but communication was not possible...

스크린샷 2023-10-14 151432.png 스크린샷 2023-10-19 202215.png
YJU by Associate
  • 3166 Views
  • 3 replies
  • 0 kudos

Resolved! LIS2HH12 working like 1.6kHz@ODR=800Hz

I am evaluating LIS2HH12. Before starting to collect data, I simply reboot it, set FIFO to stream mode (010), enable FIFO, and enable the sensor by setting ODR=800Hz (110). Then I collect 800 samples (each sample=6 bytes, 2 for each axis) by reading ...

mete by Senior II
  • 2186 Views
  • 2 replies
  • 0 kudos

Resolved! STHS34PF80 sensor with Nucleo_l073

I connected the MKI231KA board to the Nucleo-L073 board to test the STHS34PF80.And I downloaded the PresenceDetection_STHS34PF80 example in the MEMS1 package.Afterwards, I ran Unicleo-GUI and connected it to the COM port, but the data was not read No...

PatrickS by Associate
  • 3350 Views
  • 3 replies
  • 0 kudos

[LIS2DUXS12] Set FIFO_MODE when using FSM

I had an idea to start recording accelerometer data in the FIFO by switching to FIFO mode at one point in the Finite State Machine. This would be done by setting FIFO_MODE bits in the FIFO_CTRL register by using the SETR command. However, in the an59...

BD651 by Associate II
  • 1640 Views
  • 1 replies
  • 0 kudos

Pdm mems microphone

Hi team, I am using MP23DB01HP mems pdm microphone.I am new to this PDM DATA format.i know about pcm.Llease provide information and pseudo code for pdm  to pcm  and vice-versa.Waiting for ur response...!Thank u,Alex