MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Sample code for IMU

Hi ST experts,Is there any sample codes available for IMU?I checked the info of X-Cube-MEMES-XT1 is already NRND.  

STLearner by Associate III
  • 3645 Views
  • 4 replies
  • 1 kudos

Resolved! LSM6DSV FSM example with baro (LPS22XX) as external sensor?

I have examined the FSM example folder on github and, while there is an example for an external magnetometer, I haven't found any examples for an external barometer. Is there such an example? And if so, where can I find it?I believe I can create my o...

KWine by Senior
  • 2890 Views
  • 4 replies
  • 0 kudos

Resolved! reading zeroes from IIS3DWB FIFO

Sometimes, I am reading zeroes from IIS3DWB FIFO. I thought maybe it is because I am using a protoboard (using MKI208) so I connected it directly (with cables) to RPi 4 but it still happens.I guess it is not normal to find these in FIFO, can it be du...

mete by Senior II
  • 1721 Views
  • 1 replies
  • 0 kudos

Resolved! asm330lhhx scale factor for each x, y, z axis

Hello,For the asm330lhhx device, when does the scale value change and get set?  I am trying to determine if the scale factor needs to be checked only once at power up or continually while reading the raw x, y, and z values for both the gyro and the a...

Resolved! LSM6DSV Sensor Hub current consumption?

Based on power measurements I infer that using the LSM6DSV embedded SensorHub with a single slave (LPS22DF) costs ~6.4 uA. I can't find the expected current consumption for the LSM6DSV Sensor Hub in the data sheet or application notes. Is this a reas...

KWine by Senior
  • 2456 Views
  • 3 replies
  • 0 kudos

Resolved! Documentation for MEMS module

Where can I find the proper documentation for the functions in X -Cube - MEMS package and clear explanations for the use of functions

Priyaa by Associate II
  • 1388 Views
  • 1 replies
  • 0 kudos

Resolved! LIS2DUX12 not reaching current consumption said in datasheet

Hello,I'm evaluating the LIS2DUX12 accelerometer by using the combination of STEVAL-MKI109V3 and STEVAL-MKI238A. In the datasheet it stablishes that it can reach down to 10 nA during deep power-down:But when I measure the current consumption through ...

sch0bert_0-1695906333273.png sch0bert_1-1695906513982.png
sch0bert by Associate III
  • 3988 Views
  • 6 replies
  • 0 kudos

Resolved! Can't get to find how to turn off temp sensor from LIS2DUX12

Hello! I'm evaluating the LIS2DUX12 accelerometer by using the combination of STEVAL-MKI109V3 and STEVAL-MKI238A. In the datasheet it stablishes that in order to achieve certain current consumption is necessary to have the Temperature sensor off:But ...

sch0bert_0-1695906928646.png
sch0bert by Associate III
  • 3977 Views
  • 7 replies
  • 1 kudos

Resolved! LIS3DSH, SDO Pullup Register

Hello,We have been using the LIS3DH for some time and recently acquire some LIS3DSH' as well.With both modules there is an internal pull-up for the SDO pin, and with the LIS3DH there is a register to control this pullup:CTRL_REG0I am not able to find...

videojames_0-1695096274516.png

Resolved! FSM compatibility with SFLP or tap detect in LSM6DSV?

I have four FSM programs working with the LSM6DSV sensor, all set to AODR/GODR of 30Hz in line with the examples I copied. Tap detect requires significantly higher ODR.  I might also want to run the SFLP at a rate higher than 15 or 30 Hz, so does thi...

KWine by Senior
  • 2302 Views
  • 3 replies
  • 0 kudos