cancel
Showing results for 
Search instead for 
Did you mean: 

Does ISPU offer deep sleep for even more power save and what is the lowest deep sleep watt usage?

ILARIASOFIA.GRASSI
ST Employee
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Denise SANFILIPPO
ST Employee

Despite the name, when the ISPU is in "sleep" state, it is fully off. In this state, the current consumption is in the order of a few microamperes. In order to keep the ISPU fully in this state you can either set the CLK_DIS bit to 1 in the

ISPU_CONFIG register to completely disable the clock or set the ISPU IRQ rate to 0 Hz by writing ISPU_RATE_[3:0] in the CTRL9_C register to 0h.

View solution in original post

1 REPLY 1
Denise SANFILIPPO
ST Employee

Despite the name, when the ISPU is in "sleep" state, it is fully off. In this state, the current consumption is in the order of a few microamperes. In order to keep the ISPU fully in this state you can either set the CLK_DIS bit to 1 in the

ISPU_CONFIG register to completely disable the clock or set the ISPU IRQ rate to 0 Hz by writing ISPU_RATE_[3:0] in the CTRL9_C register to 0h.