MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Behaviour change when powering with external power source

Hi everyone,I am using a STWINKT1B and I am trying to evaluate its power consumption while operating. The Wifi communication always works well when I power the board by the battery or the USB port but never when I plug it to my voltage source (5V on ...

chhhhak by Associate II
  • 3442 Views
  • 6 replies
  • 0 kudos

lis302dl on STM32f407 VG Y Axis do not Change

Hello, I have been trying to make a accelerator project by using lis302dl accelorator on STM32f407 vg discovery card. There are three axis which are x, y and z. These have x, y and z variables according to position of lis302dl on the card. I have use...

Resolved! How to use LSM6DSO32X

Hi,I am using LSM6DSO32X using SPI communication in TI AM2634 Chip.By default, I made a packet of Ctrl1_xl and Ctrl2_xl to 0x10b0 0x1110, and the Accel data and GYRO data were output.I saw Datasheet, but it's too hard to understand what each register...

제목 없음.png
sygo by Associate II
  • 2682 Views
  • 5 replies
  • 0 kudos

lps33k

helloI'm currently using the LPS22DF pressure transducer, which can withstand up to 22,000 g, but since in the work environment there's dust and water, I'm going to switch to either the LPS28DFW or LPS33K since they're waterproof, but in their datash...

ljm by Associate III
  • 1242 Views
  • 0 replies
  • 0 kudos

FP-SNS-DATALOG1 DeviceConfig.json

Can i reduce the sensitivity ("sensitivity": 1) for a microphone (IMP23ABSU) for it not to reach the 130dbSPL? What does the "samplesPerTs": 1000" translate to? Is the sampling frequency defined with "ODR": 192000" or "ODRMeasured": 192000" ? What is...

TomRett_1-1699733239524.png
TomRett by Associate III
  • 1102 Views
  • 0 replies
  • 0 kudos

Resolved! Unable to write registers for the LSM6DSOX IMU sensor

I am currently working with the LSM6DSOX IMU sensor from ST and I am unable to write to registers of the sensor.I am addressing the sensor via 4 Wire SPI.For example if I try to set the output data rate which is located in the register CTRL1_XL (0x10...

Reewen_0-1698771323820.png Reewen_1-1698771469356.png
Reewen by Associate II
  • 2473 Views
  • 4 replies
  • 0 kudos

how to improve the actual ODR of LIS2DH12 ?

In my design, when setting the ODR = 100Hz or below ,  I can get 100hz INT signals , and received 100 sets vibration data every Second.  (Using XYZ data-ready as int1)and modify the ODR setting to 200Hz , just get 200 hz INT signals ,and received 145...

JohnGe by Associate
  • 1393 Views
  • 1 replies
  • 0 kudos

Resolved! ISM330DHCX: Gyro range in driver: calculation does not make sense

Greetings, I am trying to figure out the full chain scaling values for the gyro and accelerometer of the ISM330DHCX. I am reading the datasheet as well as the AN5398.  According to the datasheet the output values of accelerometer and gyro is scaled w...

GHope.2 by Associate II
  • 2552 Views
  • 2 replies
  • 1 kudos