MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

how to improve the actual ODR of LIS2DH12 ?

In my design, when setting the ODR = 100Hz or below ,  I can get 100hz INT signals , and received 100 sets vibration data every Second.  (Using XYZ data-ready as int1)and modify the ODR setting to 200Hz , just get 200 hz INT signals ,and received 145...

JohnGe by Associate
  • 878 Views
  • 1 replies
  • 0 kudos

Resolved! ISM330DHCX: Gyro range in driver: calculation does not make sense

Greetings, I am trying to figure out the full chain scaling values for the gyro and accelerometer of the ISM330DHCX. I am reading the datasheet as well as the AN5398.  According to the datasheet the output values of accelerometer and gyro is scaled w...

GHope.2 by Associate II
  • 1937 Views
  • 2 replies
  • 1 kudos

[mems] speed prediction in the tunnel

Hello,I have question about gps speed prediction in the tunnel.When gps loses signal in the tunnel, we can not get any speed info from gps.In that case, can we predict speed using mems? If yes, how to solve that?Thanks in advance for your advice.Best...

Tiel by Associate II
  • 3531 Views
  • 7 replies
  • 0 kudos

Resolved! Very noisy signal from IMP34DT05 recorded with STM32-F401RE

Hello,I'm using the IMP34DT05 available with the STEVAL-MIC003V1 kit to record audio the nucleo-f401re. I'm using the PDM2PCM library to convert the PDM stream to PCM data. The audio is recorded at 8kHz.I have tried reproducing 1kHz tone on the micro...

frnt by Senior
  • 3545 Views
  • 7 replies
  • 0 kudos

LSM6DSO Finite State Machine (FSM) Input Data

Hi,I'm doing gesture recognition with the LSM6DSO(X) finite state machine. It still doesn't work as it should.1.Can I use sqrt(x²+y²) as input data without using the z axis information? Similar to the norm sqrt(x²+y²+z²), but without z axis. I am not...

Pointes by Associate II
  • 1671 Views
  • 1 replies
  • 0 kudos

SensorTile.box PRO project in STM32CubeIDE from scratch

  Hello. I would like to make a new project for the "SensorTile.box PRO" board using STM32CubeIDE. It appears that the board is not available. (In the image below, you can see that I have filtered on "box" and only the non-pro SensorTile.box device s...

stuart_rubin_ns_0-1699030180133.png

STEVAL-MK141V2 (HTS221) temp/RH sensor

Hi, I got the reference board of STEVAL-MKI141V2 that has HTS221 temperature and humidity sensor.#1I read out the calibration registers by the manual of https://www.st.com/resource/en/technical_note/tn1218-interpreting-humidity-and-temperature-readin...

Take4az by Associate
  • 813 Views
  • 1 replies
  • 0 kudos