cancel
Showing results for 
Search instead for 
Did you mean: 

how to improve the actual ODR of LIS2DH12 ?

JohnGe
Associate

In my design, when setting the ODR = 100Hz or below ,  I can get 100hz INT signals , and received 100 sets vibration data every Second.  (Using XYZ data-ready as int1)and modify the ODR setting to 200Hz , just get 200 hz INT signals ,and received 145 sets data。

How to improve the actual ODR ?  We want  realize 1.376KHz @hr mode

 or 5.376kHz @LP mode,  Which mcu is suitable ?  STM32F103  70MHz ?  or  higher End ?   
And I2C interface is suitable for 5.376kHz ? or must be SPI ?

 

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Federica Bossi
ST Employee

Hi @JohnGe ,

You need to use SPI @ 10MHz and an powerful mcu to manage that interrupt velocity such as a STM32U5.

For further questions I suggest you to open a topic on the MCU forum.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.