MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS2DH12TR have some questions for help .

  LIS2DH12TR   have  some questions for help below: 1. The captured accelerometer data found that there was a fixed frequency of jitter, and I wanted the manufacturer to determine whether it was a problem with the hardware itself2. I would like to as...

SFLP vs MotionFX algorithm

Hi team,                 I have purchased STEVAL-MKBOXPRO, It has LSM6DSV16X IMU with SFLP algorithm. MotionFX algorithm used in Algo builder. Is there any difference between those algorithm?. Which one is give more accurate output?

Daya by Associate II
  • 1659 Views
  • 3 replies
  • 0 kudos

Resolved! lsm6dsv16bx data validation

I have integrated lsm6dsv16bx in my Microcontroller and I'm able to see the IMU datas in output for example:  AX=61,AY=-131,AZ=-997,GX=-770,GY=2380,GZ=560.I have used the example code provided in the ST's official github page(https://github.com/STMic...

Varsha by Associate III
  • 1634 Views
  • 5 replies
  • 1 kudos

How to test the IMP23ABSU MEMS

I would like to use the following MEMS microphones to test the resonance frequencies of an ultrasonic bath: https://www.st.com/en/evaluation-tools/steval-mic007v1.html#overview I would like to ask what other parts I need to convert the analog signal ...

EcoKF by Associate
  • 1393 Views
  • 3 replies
  • 1 kudos

Resolved! lis2dw12

Hello,I'm currently working with a custom board designed to read digital values from an accelerometer, specifically from the OUT_X, OUT_Y, and OUT_Z registers. However, I've encountered an issue: despite the accelerometer being physically stable, I a...

image.png
sde c.1 by Senior II
  • 2254 Views
  • 4 replies
  • 1 kudos

BlueCoin入门套件

BlueCoin入门套件使用波束形成算法时,采样率能达到多少啊 

insist_66 by Associate II
  • 1003 Views
  • 3 replies
  • 0 kudos

Resolved! Reading any register from IIS3DWB sensor only yields 11111111

Hello,I have run into an unexpected problem when trying to read registers from the IIS3DWB sensor. The setup is attached in the picture. I am using an Arduino Uno R3 and an STEVAL MKI208V1 board. The code is fairly simple so I am not sure what is goi...

xl by Associate
  • 1765 Views
  • 2 replies
  • 0 kudos

MP34DT05-A randome noise

Hello ST community,I am unfortunately facing a problem with the MP34DT05-A MEMS microphone. I am using the DFSDM module to read in the microphone. Unfortunately, it happens again and again that extremely strong noise is added at a random time (see pi...

3a9e992e-2607-47a1-a37b-e0b8182a61b5.png
ChRegBrg by Associate II
  • 2036 Views
  • 4 replies
  • 3 kudos

AcousticBF

Can the AcousticBF beamforming algorithm from FP-AUD-SMARTMIC1 algorithm be used on the entry-level kit of BlueCoin board (STEVAL-BCNCS01V1) to achieve audio acquisition at a sampling rate of 48kHz?

insist_66 by Associate II
  • 1923 Views
  • 3 replies
  • 0 kudos