MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS3MDLTR Data Ready (DRDY) on INT pin

Hi! I've got a product that we've just made a load of and while building out the firmware I realised that the INT pin on the LIS3MDLTR doesn't (at least according to the datasheet) appear to be able to be configured to show when new data is ready. Th...

gw by Associate II
  • 5209 Views
  • 4 replies
  • 0 kudos

Resolved! LIS2DH12

Guys, I ran into a strange problem while debugging LIS2DH12, someone help me. I configured the high-precision mode, using 12 bits, with a range of +-4g, that is, when I placed the table (the chip with the sign facing up, the positive direction descri...

bennanbei_0-1711373762150.png bennanbei_1-1711373806843.png bennanbei_2-1711373822879.png bennanbei_3-1711373830515.png
bennanbei by Associate II
  • 2591 Views
  • 4 replies
  • 0 kudos

LSM6DSLTR interrupt configuration

Hi, I am trying to configure interrupt on LSM6DSLTR module but I am not able to get any interrupt on the pin INT1.I am using nrf52 dk for setting interrupt on pin. err_code = nrf_drv_mpu_write_single_register(LSM6DSL_ACC_GYRO_INT1_CTRL, 0x03);if(err_...

yash2530 by Associate II
  • 3209 Views
  • 6 replies
  • 0 kudos

ISM330DLC Sensor

I have a question about the FIFO_Pattern.If I have only configured the accelerometer and set the watermark to 1536 samples, meaning 1536/3, which is equivalent to 512 samples (16 bits each sample) for each x, y, and z. And one sample is reading from ...

Resolved! Lis3MDL - SPI multiple IC bus

HiI saw that the CS and I2C enable are on the same pin and also the SPI and I2C CLK and data.Does it means that this component can not be with other SPI IC on the same line? (because when the CS is 1 while talking to other ICs it will be in I2C mode ...

orsamoo by Associate II
  • 3962 Views
  • 6 replies
  • 0 kudos

Advice - Helmet Mounted Environment and Motion Sensor

Hello,I am looking for sensors for an upcoming research experiment looking at helmet-mounted motion and environmental sensing and found this article: MEMS Accelerometer Integral To New Helmet-Mounted Impact Sensor | Electronic Design. I am not lookin...

novice by Associate
  • 1368 Views
  • 1 replies
  • 0 kudos

LSM6DSO32X Act./Inactivity max ODR

Hello, Im trying to set up Act/Inactivity INT1 at high ODR (1.66khz / 2000dps / 4g). Its threshold is too high so it resets or goes in/out of active/inactive state too often. Is there any way to lower the activity threshold so it really needs to be a...

IRogo.1 by Associate II
  • 1814 Views
  • 2 replies
  • 0 kudos

Resolved! Minimum RAM required warning

Hi, I am working on Anomaly Detection in motor using ISM330ISN. As soon as I am choosing the Buffer Size of 256 in the datalogger and adding the signal, I am getting this warning of minimum RAM required is 9KB. However upto 128 buffer size, it is wor...

jayantver_0-1716554438620.png