cancel
Showing results for 
Search instead for 
Did you mean: 

COM PORT is not detected while using STEVAL-MKSBOX1V1 (stm32l4r9zij6)

PRATIK_HALK
Associate II

"While transmission of data via the USART COM PORT is not detected, which driver should I use on windows 11  for COM PORT detection?"

 

 

i have use many drivers till now but not getting any satisfied solution.

This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
Pavel A.
Super User

Was the COM port detected before transmission of data? Usually you want the "standard" in-box driver.

PRATIK_HALK
Associate II

i was doing UART program.  

the virtual com port is detected in DEVICE MANAGER after installation of a random driver .

But its not working ..on my STM32CUBEIDE or in my TERA TERM  application ,  connection with COM PORT is failed.

suggest me a appropriate driver to solve this issue. 

 

*code is in the below section

Pavel A.
Super User

After installation of a random driver - what does this mean? What is the random driver?

 

There are so many drivers on the internet

i just download one and installed!

i get the link from a youtube video.

Peter BENSCH
ST Employee

Of course, there are many drivers available on the Internet, but it is not very helpful to install just anything. In addition, it is not clear why you want to install a COM port driver at all, since STEVAL-MKSBOX1V1 does not even provide a COM port?

Have you actually read through the documentation for STEVAL-MKSBOX1V1?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.