2024-08-14 6:52 AM
I'm trying to extract the data Game Rotation Data from the ism330bx sensor. I'm just not quite sure, which setting to use for that. What I did so far:
Setting the sensor for an ODR of 480Hz with a range of 4000dps and 8g.
(ism330bx_reset(NULL))
(ism330bx_auto_inc(NULL)) // set auto increment register
(ism330bx_set_odr_g(NULL)) // 480Hz
(ism330bx_set_range_g(NULL)) // 8g
(ism330bx_set_odr_xl(NULL)) // 480Hz
(ism330bx_set_range_xl(NULL)) // 8gAfter that I can extract the sensor data from the registers 0x22 to 0x2D.
Now I'm trying to configure the SFLP function in the embedded functions:
I2C_WRITE_PARAM writeParam = {
.Address = ISM330BX_ADDRESS,
.Data = 0b10000000,
.Register = FUNC_CFG_ACCESS
};
i2cWriteSuccess = i2c_write(&writeParam); // switches to embedded fuunctions
writeParam.Register = EMB_FUNC_EN_A;
writeParam.Data = 0b00000010;
i2cWriteSuccess = i2c_write(&writeParam); // activation of SFLP
writeParam.Register = SFLP_ODR;
writeParam.Data = 0b01101011;
i2cWriteSuccess = i2c_write(&writeParam); // ODR = 480Hz (for SFLP)
writeParam.Register = EMB_FUNC_FIFO_EN_A;
writeParam.Data = 0b00110010;
i2cWriteSuccess = i2c_write(&writeParam); // FIFO Data (GameRotVector, GBIAS, Gravity)
writeParam.Register = EMB_FUNC_INIT_A;
writeParam.Data = 0b00000010;
i2cWriteSuccess = i2c_write(&writeParam); // initialisation (für SFLP)
writeParam.Register = EMB_FUNC_EN_A;
writeParam.Data = 0b00000000;
i2cWriteSuccess = i2c_write(&writeParam); // switches back from embedded functionsFrom what I understand I have to read the SFLP data from the FIFO. However I'm not quite sure how to configure it.
1. Is there a setting (continous FIFO maybe?) to read the SFLP data easily like the sensor data? Which register do I have to use to read the FIFO and how do I know where my SFLP data is located.
2. Is there a mode to read automatically the last data stored. For example I want to do the fusion with a frequeny of 480 Hz, but I would read the data only at 5 to 10 Hz. So I would only be interested in the last calculation of the sensor fusion.
2024-08-30 3:06 AM